This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs.
A PLL will take an input signal (the source), optionally divide the frequency by a configurable divider, and then multiply the frequency by a configurable multiplier.
Some devices don't support input dividers; specifying any other divisor than 1 on these devices will result in an assertion failure. Other devices may have various restrictions to the frequency range of the input and output signals.
The following example shows how to configure and enable PLL0 using the default parameters specified using the configuration symbols listed above.
To configure, enable PLL0 using the default parameters and to disable a specific feature like Wide Bandwidth Mode (a UC3A3-specific PLL option.), you can use this initialization process.
When the last function call returns, PLL0 is ready to be used as the main system clock source.
Each PLL has a set of default parameters determined by the following configuration symbols in the application's configuration file:
These configuration symbols determine the result of calling pll_config_defaults() and pll_get_default_rate().
Data Structures | |
struct | pll_config |
Hardware-specific representation of PLL configuration. More... | |
Macros | |
#define | PLL_COUNT 0x3fU |
#define | PLL_INPUT_MAX_HZ 32000000 |
#define | PLL_INPUT_MIN_HZ 3000000 |
#define | PLL_OUTPUT_MAX_HZ 240000000 |
#define | PLL_OUTPUT_MIN_HZ 80000000 |
#define | PLLA_ID 0 |
#define | PLLB_ID 1 |
Enumerations | |
enum | pll_source { PLL_SRC_MAINCK_4M_RC = OSC_MAINCK_4M_RC, PLL_SRC_MAINCK_8M_RC = OSC_MAINCK_8M_RC, PLL_SRC_MAINCK_12M_RC = OSC_MAINCK_12M_RC, PLL_SRC_MAINCK_XTAL = OSC_MAINCK_XTAL, PLL_SRC_MAINCK_BYPASS = OSC_MAINCK_BYPASS, PLL_NR_SOURCES } |
PLL clock source. More... | |
Functions | |
static void | pll_config_init (struct pll_config *p_cfg, enum pll_source e_src, uint32_t ul_div, uint32_t ul_mul) |
static void | pll_config_read (struct pll_config *p_cfg, uint32_t ul_pll_id) |
static void | pll_config_write (const struct pll_config *p_cfg, uint32_t ul_pll_id) |
static void | pll_disable (uint32_t ul_pll_id) |
static void | pll_enable (const struct pll_config *p_cfg, uint32_t ul_pll_id) |
static uint32_t | pll_is_locked (uint32_t ul_pll_id) |
Chip-specific PLL characteristics | |
#define | NR_PLLS 2 |
Number of on-chip PLLs. More... | |
PLL configuration | |
#define | pll_config_defaults(cfg, pll_id) |
Initialize PLL configuration using default parameters. More... | |
#define | pll_get_default_rate(pll_id) |
Get the default rate in Hz of pll_id. More... | |
Interaction with the PLL hardware | |
static int | pll_wait_for_lock (unsigned int pll_id) |
Wait for PLL pll_id to become locked. More... | |
static void | pll_enable_source (enum pll_source e_src) |
Enable the source of the pll. More... | |
static void | pll_enable_config_defaults (unsigned int ul_pll_id) |
Enable the pll with the default configuration. More... | |
#define NR_PLLS 2 |
Number of on-chip PLLs.
Referenced by pll_config_read(), pll_config_write(), pll_disable(), pll_enable(), pll_is_locked(), and pll_wait_for_lock().
#define pll_config_defaults | ( | cfg, | |
pll_id | |||
) |
Initialize PLL configuration using default parameters.
After this function returns, cfg will contain a configuration which will make the PLL run at (CONFIG_PLLx_MUL / CONFIG_PLLx_DIV) times the frequency of CONFIG_PLLx_SOURCE.
cfg | The PLL configuration to be initialized. |
pll_id | Use defaults for this PLL. |
Referenced by sysclk_enable_usb(), and sysclk_init().
#define PLL_COUNT 0x3fU |
Referenced by pll_config_init().
#define pll_get_default_rate | ( | pll_id | ) |
Get the default rate in Hz of pll_id.
Referenced by sysclk_get_main_hz().
#define PLL_INPUT_MAX_HZ 32000000 |
Referenced by pll_config_init().
#define PLL_INPUT_MIN_HZ 3000000 |
Referenced by pll_config_init().
#define PLL_OUTPUT_MAX_HZ 240000000 |
Referenced by pll_config_init().
#define PLL_OUTPUT_MIN_HZ 80000000 |
Referenced by pll_config_init().
#define PLLA_ID 0 |
Referenced by pll_config_read(), pll_config_write(), pll_disable(), pll_enable(), and pll_is_locked().
#define PLLB_ID 1 |
enum pll_source |
PLL clock source.
|
inlinestatic |
References Assert, pll_config::ctrl, osc_get_rate(), PLL_COUNT, PLL_INPUT_MAX_HZ, PLL_INPUT_MIN_HZ, PLL_NR_SOURCES, PLL_OUTPUT_MAX_HZ, and PLL_OUTPUT_MIN_HZ.
Referenced by pll_enable_config_defaults().
|
inlinestatic |
References Assert, pll_config::ctrl, NR_PLLS, and PLLA_ID.
|
inlinestatic |
References Assert, pll_config::ctrl, NR_PLLS, PLLA_ID, pmc_disable_pllack(), and pmc_disable_pllbck().
|
inlinestatic |
References Assert, NR_PLLS, PLLA_ID, pmc_disable_pllack(), and pmc_disable_pllbck().
|
inlinestatic |
References Assert, pll_config::ctrl, NR_PLLS, PLLA_ID, pmc_disable_pllack(), and pmc_disable_pllbck().
Referenced by pll_enable_config_defaults(), sysclk_enable_usb(), and sysclk_init().
|
inlinestatic |
Enable the pll with the default configuration.
PLL is enabled, if the PLL is not already locked.
pll_id | The ID of the PLL to enable. |
References Assert, CONFIG_PLL1_DIV, CONFIG_PLL1_MUL, CONFIG_PLL1_SOURCE, pll_config_init(), pll_enable(), pll_enable_source(), and pll_is_locked().
Referenced by genclk_enable_source().
|
inlinestatic |
Enable the source of the pll.
The source is enabled, if the source is not already running.
src | The ID of the PLL source to enable. |
References Assert, osc_enable(), osc_wait_ready(), PLL_SRC_MAINCK_12M_RC, PLL_SRC_MAINCK_4M_RC, PLL_SRC_MAINCK_8M_RC, PLL_SRC_MAINCK_BYPASS, and PLL_SRC_MAINCK_XTAL.
Referenced by pll_enable_config_defaults(), sysclk_enable_usb(), and sysclk_init().
|
inlinestatic |
References Assert, NR_PLLS, PLLA_ID, pmc_is_locked_pllack(), and pmc_is_locked_pllbck().
Referenced by pll_enable_config_defaults(), and pll_wait_for_lock().
|
inlinestatic |
Wait for PLL pll_id to become locked.
pll_id | The ID of the PLL to wait for. |
STATUS_OK | The PLL is now locked. |
ERR_TIMEOUT | Timed out waiting for PLL to become locked. |
References Assert, NR_PLLS, and pll_is_locked().
Referenced by sysclk_enable_usb(), and sysclk_init().