Purpose
The example demonstrates how to use ABDAC driver to transfers an input buffer of audio samples to an output .
Requirements
This example can be used on SAM4L-EK boards with hardware rework. Please see detail in document: ATSAM4L-EK User Guide.
Description
The example read the audio samples and output it.
Usage
- On the computer, open and configure a terminal application (e.g., HyperTerminal on Microsoft Windows) with these settings:
- 115200 bauds
- 8 bits of data
- No parity
- 1 stop bit
- No flow control
- In the terminal window, the following text should appear (values depend on the board and chip used):
-- ABDAC Example xxx --
-- xxxxxx-xx
-- Compiled: xxx xx xxxx xx:xx:xx --
- the sent text should appear.