This is the unit test application for the ABDAC driver. It contains two test case for the ABDACB module:
Only devices with ABDAC module can be used. This example has been tested with the following setup:
This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.
For further information, visit Microchip.