Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Analog-to-digital Converter (ADC)

See Quickstart guide for SAM ADC driver.

Driver for the Analog-to-digital Converter. This driver provides access to the main features of the ADC controller.

Macros

#define ADC_WPMR_WPKEY_PASSWD   ADC_WPMR_WPKEY(0x414443u)
 

Functions

void adc_check (Adc *p_adc, const uint32_t ul_mck)
 Check ADC configurations. More...
 
void adc_configure_power_save (Adc *p_adc, const uint8_t uc_sleep, const uint8_t uc_fwup)
 Configures ADC power saving mode. More...
 
void adc_configure_sequence (Adc *p_adc, const enum adc_channel_num_t ch_list[], uint8_t uc_num)
 Configure conversion sequence. More...
 
void adc_configure_timing (Adc *p_adc, const uint8_t uc_tracking, const enum adc_settling_time_t settling, const uint8_t uc_transfer)
 Configure ADC timing. More...
 
void adc_configure_trigger (Adc *p_adc, const enum adc_trigger_t trigger, uint8_t uc_freerun)
 Configure conversion trigger and free run mode. More...
 
void adc_configure_ts_comparison (Adc *p_adc, enum adc_temp_cmp_mode mode, uint16_t low_threshold, uint16_t high_threshold)
 Configure temperature sensor comparison. More...
 
void adc_disable_all_channel (Adc *p_adc)
 Disable all ADC channel. More...
 
void adc_disable_anch (Adc *p_adc)
 Disable analog change. More...
 
void adc_disable_channel (Adc *p_adc, const enum adc_channel_num_t adc_ch)
 Disable the specified ADC channel. More...
 
void adc_disable_channel_differential_input (Adc *p_adc, const enum adc_channel_num_t channel)
 Disable differential input for the specified channel. More...
 
void adc_disable_channel_input_offset (Adc *p_adc, const enum adc_channel_num_t channel)
 Disable analog signal offset for the specified channel. More...
 
void adc_disable_interrupt (Adc *p_adc, const uint32_t ul_source)
 Disable ADC interrupts. More...
 
void adc_disable_tag (Adc *p_adc)
 Disable TAG option. More...
 
void adc_disable_ts (Adc *p_adc)
 Turn off temperature sensor. More...
 
void adc_enable_all_channel (Adc *p_adc)
 Enable all ADC channels. More...
 
void adc_enable_anch (Adc *p_adc)
 Enable analog change. More...
 
void adc_enable_channel (Adc *p_adc, const enum adc_channel_num_t adc_ch)
 Enable the specified ADC channel. More...
 
void adc_enable_channel_differential_input (Adc *p_adc, const enum adc_channel_num_t channel)
 Enable differential input for the specified channel. More...
 
void adc_enable_channel_input_offset (Adc *p_adc, const enum adc_channel_num_t channel)
 Enable analog signal offset for the specified channel. More...
 
void adc_enable_interrupt (Adc *p_adc, const uint32_t ul_source)
 Enable ADC interrupts. More...
 
void adc_enable_tag (Adc *p_adc)
 Enable TAG option so that the number of the last converted channel can be indicated. More...
 
void adc_enable_ts (Adc *p_adc)
 Turn on temperature sensor. More...
 
uint32_t adc_get_actual_adc_clock (const Adc *p_adc, const uint32_t ul_mck)
 Return the actual ADC clock. More...
 
uint32_t adc_get_channel_status (const Adc *p_adc, const enum adc_channel_num_t adc_ch)
 Read the ADC channel status. More...
 
uint32_t adc_get_channel_value (const Adc *p_adc, const enum adc_channel_num_t adc_ch)
 Read the ADC result data of the specified channel. More...
 
uint32_t adc_get_comparison_mode (const Adc *p_adc)
 Get comparison mode. More...
 
uint32_t adc_get_interrupt_mask (const Adc *p_adc)
 Read ADC interrupt mask. More...
 
uint32_t adc_get_latest_value (const Adc *p_adc)
 Read the last ADC result data. More...
 
uint32_t adc_get_overrun_status (const Adc *p_adc)
 Get ADC interrupt and overrun error status. More...
 
Pdc * adc_get_pdc_base (const Adc *p_adc)
 Get PDC registers base address. More...
 
uint32_t adc_get_status (const Adc *p_adc)
 Get ADC interrupt and overrun error status. More...
 
enum adc_channel_num_t adc_get_tag (const Adc *p_adc)
 Indicate the last converted channel. More...
 
uint32_t adc_get_writeprotect_status (const Adc *p_adc)
 Indicate write protect status. More...
 
uint32_t adc_init (Adc *p_adc, const uint32_t ul_mck, const uint32_t ul_adc_clock, const enum adc_startup_time startup)
 Initialize the given ADC with the specified ADC clock and startup time. More...
 
void adc_reset (Adc *p_adc)
 Reset ADC. More...
 
void adc_set_averaging_trigger (Adc *p_adc, bool multi)
 Set digital averaging trigger. More...
 
void adc_set_bias_current (Adc *p_adc, const uint8_t uc_ibctl)
 Adapt performance versus power consumption. More...
 
void adc_set_calibmode (Adc *p_adc)
 Set ADC auto calibration mode. More...
 
void adc_set_channel_input_gain (Adc *p_adc, const enum adc_channel_num_t channel, const enum adc_gainvalue_t gain)
 Configure input gain for the specified channel. More...
 
void adc_set_comparison_channel (Adc *p_adc, const enum adc_channel_num_t channel)
 Configure comparison selected channel. More...
 
void adc_set_comparison_filter (Adc *p_adc, uint8_t filter)
 Set comparison filter. More...
 
void adc_set_comparison_mode (Adc *p_adc, const uint8_t uc_mode)
 Configure comparison mode. More...
 
void adc_set_comparison_window (Adc *p_adc, const uint16_t us_low_threshold, const uint16_t us_high_threshold)
 Configure ADC compare window. More...
 
enum status_code adc_set_internal_reference_voltage (Adc *p_adc, struct adc_internal_ref *ref)
 Set ADC analog control(internal reference voltage). More...
 
void adc_set_resolution (Adc *p_adc, const enum adc_resolution_t resolution)
 Configure the conversion resolution. More...
 
void adc_set_writeprotect (Adc *p_adc, const uint32_t ul_enable)
 Enable or disable write protection of ADC registers. More...
 
void adc_start (Adc *p_adc)
 Start analog-to-digital conversion. More...
 
void adc_start_sequencer (Adc *p_adc)
 Enable conversion sequencer. More...
 
void adc_stop_sequencer (Adc *p_adc)
 Disable conversion sequencer. More...
 
static uint32_t calcul_startup (const uint32_t ul_startup)
 calcul_startup More...
 

#define ADC_WPMR_WPKEY_PASSWD   ADC_WPMR_WPKEY(0x414443u)

Referenced by adc_set_writeprotect().

void adc_check ( Adc *  p_adc,
const uint32_t  ul_mck 
)

Check ADC configurations.

Parameters
p_adcPointer to an ADC instance.
ul_mckMain clock of the device (in Hz).

References ADC_FREQ_MAX, ADC_FREQ_MIN, ADC_STARTUP_FAST, ADC_STARTUP_NORM, and calcul_startup().

Referenced by main().

void adc_configure_power_save ( Adc *  p_adc,
const uint8_t  uc_sleep,
const uint8_t  uc_fwup 
)

Configures ADC power saving mode.

Parameters
p_adcPointer to an ADC instance.
uc_sleepADC_MR_SLEEP_NORMAL keeps the ADC Core and reference voltage circuitry ON between conversions. ADC_MR_SLEEP_SLEEP keeps the ADC Core and reference voltage circuitry OFF between conversions.
uc_fwupADC_MR_FWUP_OFF configures sleep mode as uc_sleep setting, ADC_MR_FWUP_ON keeps voltage reference ON and ADC Core OFF between conversions.
void adc_configure_sequence ( Adc *  p_adc,
const enum adc_channel_num_t  ch_list[],
uint8_t  uc_num 
)

Configure conversion sequence.

Parameters
p_adcPointer to an ADC instance.
ch_listChannel sequence list.
numberNumber of channels in the list.
void adc_configure_timing ( Adc *  p_adc,
const uint8_t  uc_tracking,
const enum adc_settling_time_t  settling,
const uint8_t  uc_transfer 
)

Configure ADC timing.

Parameters
p_adcPointer to an ADC instance.
uc_trackingADC tracking time = uc_tracking / ADC clock.
uc_settlingAnalog settling time = (uc_settling + 1) / ADC clock.
uc_transferData transfer time = (uc_transfer * 2 + 3) / ADC clock.

Referenced by main().

void adc_configure_trigger ( Adc *  p_adc,
const enum adc_trigger_t  trigger,
uint8_t  uc_freerun 
)

Configure conversion trigger and free run mode.

Parameters
p_adcPointer to an ADC instance.
triggerConversion trigger.
uc_freerunADC_MR_FREERUN_ON enables freerun mode, ADC_MR_FREERUN_OFF disables freerun mode.

Referenced by main().

void adc_configure_ts_comparison ( Adc *  p_adc,
enum adc_temp_cmp_mode  mode,
uint16_t  low_threshold,
uint16_t  high_threshold 
)

Configure temperature sensor comparison.

Parameters
p_adcPointer to an ADC instance.
modeTemperature comparison mode.
low_thresholdTemperature low threshold.
high_thresholdTemperature high threshold.
void adc_disable_all_channel ( Adc *  p_adc)

Disable all ADC channel.

Parameters
p_adcPointer to an ADC instance.
void adc_disable_anch ( Adc *  p_adc)

Disable analog change.

Note
DIFF0, GAIN0 and OFF0 are used for all channels.
Parameters
p_AdcPointer to an ADC instance.
void adc_disable_channel ( Adc *  p_adc,
const enum adc_channel_num_t  adc_ch 
)

Disable the specified ADC channel.

Parameters
p_adcPointer to an ADC instance.
adc_chADC channel number.
void adc_disable_channel_differential_input ( Adc *  p_adc,
const enum adc_channel_num_t  channel 
)

Disable differential input for the specified channel.

Parameters
p_adcPointer to an ADC instance.
channelADC channel number.
void adc_disable_channel_input_offset ( Adc *  p_adc,
const enum adc_channel_num_t  channel 
)

Disable analog signal offset for the specified channel.

Parameters
p_adcPointer to an ADC instance.
channelADC channel number.
void adc_disable_interrupt ( Adc *  p_adc,
const uint32_t  ul_source 
)

Disable ADC interrupts.

Parameters
p_adcPointer to an ADC instance.
ul_sourceInterrupts to be disabled.

Referenced by ADC_Handler().

void adc_disable_tag ( Adc *  p_adc)

Disable TAG option.

Parameters
p_adcPointer to an ADC instance.
void adc_disable_ts ( Adc *  p_adc)

Turn off temperature sensor.

Parameters
p_adcPointer to an ADC instance.
void adc_enable_all_channel ( Adc *  p_adc)

Enable all ADC channels.

Parameters
p_adcPointer to an ADC instance.
void adc_enable_anch ( Adc *  p_adc)

Enable analog change.

Note
It allows different analog settings for each channel.
Parameters
p_AdcPointer to an ADC instance.
void adc_enable_channel ( Adc *  p_adc,
const enum adc_channel_num_t  adc_ch 
)

Enable the specified ADC channel.

Parameters
p_adcPointer to an ADC instance.
adc_chADC channel number.

Referenced by main().

void adc_enable_channel_differential_input ( Adc *  p_adc,
const enum adc_channel_num_t  channel 
)

Enable differential input for the specified channel.

Parameters
p_adcPointer to an ADC instance.
channelADC channel number.
void adc_enable_channel_input_offset ( Adc *  p_adc,
const enum adc_channel_num_t  channel 
)

Enable analog signal offset for the specified channel.

Parameters
p_adcPointer to an ADC instance.
channelADC channel number.
void adc_enable_interrupt ( Adc *  p_adc,
const uint32_t  ul_source 
)

Enable ADC interrupts.

Parameters
p_adcPointer to an ADC instance.
ul_sourceInterrupts to be enabled.

Referenced by enter_asleep().

void adc_enable_tag ( Adc *  p_adc)

Enable TAG option so that the number of the last converted channel can be indicated.

Parameters
p_adcPointer to an ADC instance.
void adc_enable_ts ( Adc *  p_adc)

Turn on temperature sensor.

Parameters
p_adcPointer to an ADC instance.
uint32_t adc_get_actual_adc_clock ( const Adc *  p_adc,
const uint32_t  ul_mck 
)

Return the actual ADC clock.

Parameters
p_adcPointer to an ADC instance.
ul_mckMain clock of the device (in Hz).
Returns
The actual ADC clock (in Hz).
uint32_t adc_get_channel_status ( const Adc *  p_adc,
const enum adc_channel_num_t  adc_ch 
)

Read the ADC channel status.

Parameters
p_adcPointer to an ADC instance.
adc_chADC channel number.
Return values
1if channel is enabled.
0if channel is disabled.
uint32_t adc_get_channel_value ( const Adc *  p_adc,
const enum adc_channel_num_t  adc_ch 
)

Read the ADC result data of the specified channel.

Parameters
p_adcPointer to an ADC instance.
adc_chADC channel number.
Returns
ADC value of the specified channel.

Referenced by ADC_Handler(), display_info(), and main().

uint32_t adc_get_comparison_mode ( const Adc *  p_adc)

Get comparison mode.

Parameters
p_adcPointer to an ADC instance.
Return values
Comparemode value.

Referenced by ADC_Handler(), and get_comparison_mode().

uint32_t adc_get_interrupt_mask ( const Adc *  p_adc)

Read ADC interrupt mask.

Parameters
p_adcPointer to an ADC instance.
Returns
The interrupt mask value.
uint32_t adc_get_latest_value ( const Adc *  p_adc)

Read the last ADC result data.

Parameters
p_adcPointer to an ADC instance.
Returns
ADC latest value.
uint32_t adc_get_overrun_status ( const Adc *  p_adc)

Get ADC interrupt and overrun error status.

Parameters
p_adcPointer to an ADC instance.
Returns
ADC status structure.
Pdc* adc_get_pdc_base ( const Adc *  p_adc)

Get PDC registers base address.

Parameters
p_adcPointer to an ADC instance.
Returns
ADC PDC register base address.

References UNUSED.

uint32_t adc_get_status ( const Adc *  p_adc)

Get ADC interrupt and overrun error status.

Parameters
p_adcPointer to an ADC instance.
Returns
ADC status structure.

Referenced by ADC_Handler(), and enter_asleep().

enum adc_channel_num_t adc_get_tag ( const Adc *  p_adc)

Indicate the last converted channel.

Note
If TAG option is NOT enabled before, an incorrect channel number is returned.
Parameters
p_adcPointer to an ADC instance.
Returns
The last converted channel number.
uint32_t adc_get_writeprotect_status ( const Adc *  p_adc)

Indicate write protect status.

Parameters
p_adcPointer to an ADC instance.
Returns
0 if no write protect violation occurred, or 16-bit write protect violation source.
uint32_t adc_init ( Adc *  p_adc,
const uint32_t  ul_mck,
const uint32_t  ul_adc_clock,
const enum adc_startup_time  startup 
)

Initialize the given ADC with the specified ADC clock and startup time.

Parameters
p_adcPointer to an ADC instance.
ul_mckMain clock of the device (value in Hz).
ul_adc_clockAnalog-to-Digital conversion clock (value in Hz).
uc_startupADC start up time. Please refer to the product datasheet for details.
Returns
0 on success.

Referenced by main().

void adc_reset ( Adc *  p_adc)

Reset ADC.

Parameters
p_adcPointer to an ADC instance.
void adc_set_averaging_trigger ( Adc *  p_adc,
bool  multi 
)

Set digital averaging trigger.

Parameters
p_adcPointer to an ADC instance.
multiThe average requests several trigger events if true. The average requests only one trigger event.
void adc_set_bias_current ( Adc *  p_adc,
const uint8_t  uc_ibctl 
)

Adapt performance versus power consumption.

Note
Please refer to ADC Characteristics in the product datasheet for more details.
Parameters
p_adcPointer to an ADC instance.
ibctlADC Bias current control.
void adc_set_calibmode ( Adc *  p_adc)

Set ADC auto calibration mode.

Parameters
p_adcPointer to an ADC instance.
void adc_set_channel_input_gain ( Adc *  p_adc,
const enum adc_channel_num_t  channel,
const enum adc_gainvalue_t  gain 
)

Configure input gain for the specified channel.

Parameters
p_adcPointer to an ADC instance.
channelADC channel number.
gainGain value for the input.
void adc_set_comparison_channel ( Adc *  p_adc,
const enum adc_channel_num_t  channel 
)

Configure comparison selected channel.

Parameters
p_adcPointer to an ADC instance.
channelADC channel number.

Referenced by main().

void adc_set_comparison_filter ( Adc *  p_adc,
uint8_t  filter 
)

Set comparison filter.

Parameters
p_adcPointer to an ADC instance.
filterNumber of consecutive compare events necessary to raise the flag = filter + 1.
void adc_set_comparison_mode ( Adc *  p_adc,
const uint8_t  uc_mode 
)

Configure comparison mode.

Parameters
p_adcPointer to an ADC instance.
uc_modeADC comparison mode.

Referenced by main().

void adc_set_comparison_window ( Adc *  p_adc,
const uint16_t  us_low_threshold,
const uint16_t  us_high_threshold 
)

Configure ADC compare window.

Parameters
p_adcPointer to an ADC instance.
w_low_thresholdLow threshold of compare window.
w_high_thresholdHigh threshold of compare window.

Referenced by main().

enum status_code adc_set_internal_reference_voltage ( Adc *  p_adc,
struct adc_internal_ref ref 
)

Set ADC analog control(internal reference voltage).

Parameters
p_adcPointer to an ADC instance.
refPointer to an ADC internal reference voltage setup.
Returns
ERR_INVALID_ARG if the argument is invalid, STATUS_OK otherwise.

References adc_internal_ref::adc_force_internal_ref, adc_internal_ref::adc_internal_ref_change_enable, adc_internal_ref::adc_internal_ref_on, ERR_INVALID_ARG, STATUS_OK, and adc_internal_ref::volt.

void adc_set_resolution ( Adc *  p_adc,
const enum adc_resolution_t  resolution 
)

Configure the conversion resolution.

Parameters
p_adcPointer to an ADC instance.
resolutionADC resolution.

References ADC_10_BITS, and ADC_12_BITS.

void adc_set_writeprotect ( Adc *  p_adc,
const uint32_t  ul_enable 
)

Enable or disable write protection of ADC registers.

Parameters
p_adcPointer to an ADC instance.
ul_enable1 to enable, 0 to disable.

References ADC_WPMR_WPKEY_PASSWD.

void adc_start ( Adc *  p_adc)

Start analog-to-digital conversion.

Note
If one of the hardware event is selected as ADC trigger, this function can NOT start analog to digital conversion.
Parameters
p_adcPointer to an ADC instance.
void adc_start_sequencer ( Adc *  p_adc)

Enable conversion sequencer.

Parameters
p_adcPointer to an ADC instance.
void adc_stop_sequencer ( Adc *  p_adc)

Disable conversion sequencer.

Parameters
p_adcPointer to an ADC instance.
static uint32_t calcul_startup ( const uint32_t  ul_startup)
static

calcul_startup

Referenced by adc_check().