Microchip® Advanced Software Framework

afec.h File Reference

Analog-Front-End Controller driver for SAM.

Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"
#include "status_codes.h"

Data Structures

struct  afec_ch_config
 AFEC channel configuration structure. More...
 
struct  afec_config
 Analog-Front-End Controller configuration structure. More...
 
struct  afec_temp_sensor_config
 AFEC Temperature Sensor configuration structure. More...
 

Typedefs

typedef void(* afec_callback_t )(void)
 

Enumerations

enum  afec_cmp_mode {
  AFEC_CMP_MODE_0 = AFEC_EMR_CMPMODE_LOW,
  AFEC_CMP_MODE_1 = AFEC_EMR_CMPMODE_HIGH,
  AFEC_CMP_MODE_2 = AFEC_EMR_CMPMODE_IN,
  AFEC_CMP_MODE_3 = AFEC_EMR_CMPMODE_OUT
}
 Definitions for Comparison Mode. More...
 
enum  afec_gainvalue {
  AFEC_GAINVALUE_0 = 0,
  AFEC_GAINVALUE_1 = 1,
  AFEC_GAINVALUE_2 = 2,
  AFEC_GAINVALUE_3 = 3
}
 Definitions for AFEC gain value. More...
 
enum  afec_power_mode {
  AFEC_POWER_MODE_0 = 0,
  AFEC_POWER_MODE_1,
  AFEC_POWER_MODE_2
}
 Definitions for AFEC power mode. More...
 
enum  afec_resolution {
  AFEC_12_BITS = AFEC_EMR_RES_NO_AVERAGE,
  AFEC_13_BITS = AFEC_EMR_RES_OSR4,
  AFEC_14_BITS = AFEC_EMR_RES_OSR16,
  AFEC_15_BITS = AFEC_EMR_RES_OSR64,
  AFEC_16_BITS = AFEC_EMR_RES_OSR256
}
 Definitions for AFEC resolution. More...
 
enum  afec_startup_time {
  AFEC_STARTUP_TIME_0 = AFEC_MR_STARTUP_SUT0,
  AFEC_STARTUP_TIME_1 = AFEC_MR_STARTUP_SUT8,
  AFEC_STARTUP_TIME_2 = AFEC_MR_STARTUP_SUT16,
  AFEC_STARTUP_TIME_3 = AFEC_MR_STARTUP_SUT24,
  AFEC_STARTUP_TIME_4 = AFEC_MR_STARTUP_SUT64,
  AFEC_STARTUP_TIME_5 = AFEC_MR_STARTUP_SUT80,
  AFEC_STARTUP_TIME_6 = AFEC_MR_STARTUP_SUT96,
  AFEC_STARTUP_TIME_7 = AFEC_MR_STARTUP_SUT112,
  AFEC_STARTUP_TIME_8 = AFEC_MR_STARTUP_SUT512,
  AFEC_STARTUP_TIME_9 = AFEC_MR_STARTUP_SUT576,
  AFEC_STARTUP_TIME_10 = AFEC_MR_STARTUP_SUT640,
  AFEC_STARTUP_TIME_11 = AFEC_MR_STARTUP_SUT704,
  AFEC_STARTUP_TIME_12 = AFEC_MR_STARTUP_SUT768,
  AFEC_STARTUP_TIME_13 = AFEC_MR_STARTUP_SUT832,
  AFEC_STARTUP_TIME_14 = AFEC_MR_STARTUP_SUT896,
  AFEC_STARTUP_TIME_15 = AFEC_MR_STARTUP_SUT960
}
 Definitions for AFEC Start Up Time. More...
 
enum  afec_temp_cmp_mode {
  AFEC_TEMP_CMP_MODE_0 = AFEC_TEMPMR_TEMPCMPMOD_LOW,
  AFEC_TEMP_CMP_MODE_1 = AFEC_TEMPMR_TEMPCMPMOD_HIGH,
  AFEC_TEMP_CMP_MODE_2 = AFEC_TEMPMR_TEMPCMPMOD_IN,
  AFEC_TEMP_CMP_MODE_3 = AFEC_TEMPMR_TEMPCMPMOD_OUT
}
 Definitions for Temperature Comparison Mode. More...
 
enum  afec_trigger {
  AFEC_TRIG_SW = AFEC_MR_TRGEN_DIS,
  AFEC_TRIG_EXT = AFEC_MR_TRGSEL_AFEC_TRIG0 | AFEC_MR_TRGEN,
  AFEC_TRIG_TIO_CH_0 = AFEC_MR_TRGSEL_AFEC_TRIG1 | AFEC_MR_TRGEN,
  AFEC_TRIG_TIO_CH_1 = AFEC_MR_TRGSEL_AFEC_TRIG2 | AFEC_MR_TRGEN,
  AFEC_TRIG_TIO_CH_2 = AFEC_MR_TRGSEL_AFEC_TRIG3 | AFEC_MR_TRGEN,
  AFEC_TRIG_PWM_EVENT_LINE_0 = AFEC_MR_TRGSEL_AFEC_TRIG4 | AFEC_MR_TRGEN,
  AFEC_TRIG_PWM_EVENT_LINE_1 = AFEC_MR_TRGSEL_AFEC_TRIG5 | AFEC_MR_TRGEN,
  AFEC_TRIG_ANALOG_COMPARATOR = AFEC_MR_TRGSEL_AFEC_TRIG6 | AFEC_MR_TRGEN,
  AFEC_TRIG_FREERUN = 0xFF
}
 Definitions for AFEC trigger. More...
 

Functions

void afec_ch_get_config_defaults (struct afec_ch_config *const cfg)
 Get the AFEC channel default configurations. More...
 
static void afec_ch_sanity_check (Afec *const afec, const enum afec_channel_num channel)
 AFEC channel sanity check. More...
 
void afec_ch_set_config (Afec *const afec, const enum afec_channel_num channel, struct afec_ch_config *config)
 Configure the AFEC channel. More...
 
static void afec_channel_disable (Afec *const afec, const enum afec_channel_num afec_ch)
 Disable the specified AFEC channel. More...
 
static void afec_channel_enable (Afec *const afec, const enum afec_channel_num afec_ch)
 Enable the specified AFEC channel. More...
 
static uint32_t afec_channel_get_status (Afec *const afec, const enum afec_channel_num afec_ch)
 Get the AFEC channel status. More...
 
static uint32_t afec_channel_get_value (Afec *const afec, enum afec_channel_num afec_ch)
 Read the Converted Data of the selected channel. More...
 
static void afec_channel_set_analog_offset (Afec *const afec, enum afec_channel_num afec_ch, uint16_t aoffset)
 Set analog offset to be used for channel CSEL. More...
 
void afec_configure_sequence (Afec *const afec, const enum afec_channel_num ch_list[], const uint8_t uc_num)
 Configure conversion sequence. More...
 
void afec_disable (Afec *const afec)
 Disable AFEC Module. More...
 
void afec_disable_interrupt (Afec *const afec, enum afec_interrupt_source interrupt_source)
 Disable AFEC interrupts. More...
 
void afec_enable (Afec *const afec)
 Enable AFEC Module. More...
 
void afec_enable_interrupt (Afec *const afec, enum afec_interrupt_source interrupt_source)
 Enable AFEC interrupts. More...
 
static enum afec_cmp_mode afec_get_comparison_mode (Afec *const afec)
 Get comparison mode. More...
 
void afec_get_config_defaults (struct afec_config *const cfg)
 Get the AFEC default configurations. More...
 
static uint32_t afec_get_interrupt_mask (Afec *const afec)
 Get AFEC interrupt mask. More...
 
static uint32_t afec_get_interrupt_status (Afec *const afec)
 Get AFEC interrupt status. More...
 
static uint32_t afec_get_latest_chan_num (Afec *const afec)
 Get the Last Converted Channel Number. More...
 
static uint32_t afec_get_latest_value (Afec *const afec)
 Get the Last Data Converted. More...
 
static uint32_t afec_get_overrun_status (Afec *const afec)
 Get AFEC overrun error status. More...
 
static uint32_t afec_get_writeprotect_status (Afec *const afec)
 Indicate write protect status. More...
 
enum status_code afec_init (Afec *const afec, struct afec_config *const config)
 Initialize the AFEC Module. More...
 
void afec_set_callback (Afec *const afec, enum afec_interrupt_source source, afec_callback_t callback, uint8_t irq_level)
 Set callback for AFEC. More...
 
void afec_set_comparison_mode (Afec *const afec, const enum afec_cmp_mode mode, const enum afec_channel_num channel, uint8_t cmp_filter)
 Configure comparison mode. More...
 
static void afec_set_comparison_window (Afec *const afec, const uint16_t us_low_threshold, const uint16_t us_high_threshold)
 Configure AFEC compare window. More...
 
void afec_set_power_mode (Afec *const afec, const enum afec_power_mode mode)
 Configure AFEC power mode. More...
 
static void afec_set_resolution (Afec *const afec, const enum afec_resolution res)
 Configure conversion resolution. More...
 
static void afec_set_trigger (Afec *const afec, const enum afec_trigger trigger)
 Configure conversion trigger and free run mode. More...
 
static void afec_set_writeprotect (Afec *const afec, const bool is_enable)
 Enable or disable write protection of AFEC registers. More...
 
static void afec_start_software_conversion (Afec *const afec)
 Start analog-to-digital conversion. More...
 
void afec_temp_sensor_get_config_defaults (struct afec_temp_sensor_config *const cfg)
 Get the AFEC Temperature Sensor default configurations. More...
 
void afec_temp_sensor_set_config (Afec *const afec, struct afec_temp_sensor_config *config)
 Configure the AFEC temperature sensor. More...
 

typedef void(* afec_callback_t)(void)

Definitions for Comparison Mode.

Enumerator
AFEC_CMP_MODE_0 
AFEC_CMP_MODE_1 
AFEC_CMP_MODE_2 
AFEC_CMP_MODE_3 

Definitions for AFEC gain value.

Enumerator
AFEC_GAINVALUE_0 
AFEC_GAINVALUE_1 
AFEC_GAINVALUE_2 
AFEC_GAINVALUE_3 

Definitions for AFEC power mode.

Enumerator
AFEC_POWER_MODE_0 
AFEC_POWER_MODE_1 
AFEC_POWER_MODE_2 

Definitions for AFEC resolution.

Enumerator
AFEC_12_BITS 
AFEC_13_BITS 
AFEC_14_BITS 
AFEC_15_BITS 
AFEC_16_BITS 

Definitions for AFEC Start Up Time.

Enumerator
AFEC_STARTUP_TIME_0 
AFEC_STARTUP_TIME_1 
AFEC_STARTUP_TIME_2 
AFEC_STARTUP_TIME_3 
AFEC_STARTUP_TIME_4 
AFEC_STARTUP_TIME_5 
AFEC_STARTUP_TIME_6 
AFEC_STARTUP_TIME_7 
AFEC_STARTUP_TIME_8 
AFEC_STARTUP_TIME_9 
AFEC_STARTUP_TIME_10 
AFEC_STARTUP_TIME_11 
AFEC_STARTUP_TIME_12 
AFEC_STARTUP_TIME_13 
AFEC_STARTUP_TIME_14 
AFEC_STARTUP_TIME_15 

Definitions for Temperature Comparison Mode.

Enumerator
AFEC_TEMP_CMP_MODE_0 
AFEC_TEMP_CMP_MODE_1 
AFEC_TEMP_CMP_MODE_2 
AFEC_TEMP_CMP_MODE_3 

Definitions for AFEC trigger.

Enumerator
AFEC_TRIG_SW 
AFEC_TRIG_EXT 
AFEC_TRIG_TIO_CH_0 
AFEC_TRIG_TIO_CH_1 
AFEC_TRIG_TIO_CH_2 
AFEC_TRIG_PWM_EVENT_LINE_0 
AFEC_TRIG_PWM_EVENT_LINE_1 
AFEC_TRIG_ANALOG_COMPARATOR 
AFEC_TRIG_FREERUN 

static void afec_ch_sanity_check ( Afec *const  afec,
const enum afec_channel_num  channel 
)
inlinestatic

AFEC channel sanity check.

Parameters
afecBase address of the AFEC.
channelAFEC channel number.

References Assert, and UNUSED.

Referenced by afec_ch_set_config(), afec_channel_disable(), afec_channel_enable(), afec_channel_get_status(), afec_channel_get_value(), afec_channel_set_analog_offset(), and afec_set_comparison_mode().

static void afec_channel_disable ( Afec *const  afec,
const enum afec_channel_num  afec_ch 
)
inlinestatic

Disable the specified AFEC channel.

Parameters
afecBase address of the AFEC.
afec_chAFEC channel number.

References afec_ch_sanity_check().

static void afec_channel_enable ( Afec *const  afec,
const enum afec_channel_num  afec_ch 
)
inlinestatic

Enable the specified AFEC channel.

Parameters
afecBase address of the AFEC.
afec_chAFEC channel number.

References afec_ch_sanity_check().

static uint32_t afec_channel_get_status ( Afec *const  afec,
const enum afec_channel_num  afec_ch 
)
inlinestatic

Get the AFEC channel status.

Parameters
afecBase address of the AFEC.
afec_chAFEC channel number.
Return values
1if channel is enabled.
0if channel is disabled.

References afec_ch_sanity_check().

static uint32_t afec_channel_get_value ( Afec *const  afec,
enum afec_channel_num  afec_ch 
)
inlinestatic

Read the Converted Data of the selected channel.

Parameters
afecBase address of the AFEC.
afec_chAFEC channel number.
Returns
AFEC converted value of the selected channel.

References afec_ch_sanity_check().

Referenced by afec_temp_sensor_end_conversion().

static void afec_channel_set_analog_offset ( Afec *const  afec,
enum afec_channel_num  afec_ch,
uint16_t  aoffset 
)
inlinestatic

Set analog offset to be used for channel CSEL.

Parameters
afecBase address of the AFEC.
afec_chAFEC channel number.
aoffsetAnalog offset value.

References afec_ch_sanity_check().

Referenced by main().

static enum afec_cmp_mode afec_get_comparison_mode ( Afec *const  afec)
inlinestatic

Get comparison mode.

Parameters
afecBase address of the AFEC.
Return values
Comparemode value.
static uint32_t afec_get_interrupt_mask ( Afec *const  afec)
inlinestatic

Get AFEC interrupt mask.

Parameters
afecBase address of the AFEC.
Returns
The interrupt mask value.

Referenced by afec_process_callback().

static uint32_t afec_get_interrupt_status ( Afec *const  afec)
inlinestatic

Get AFEC interrupt status.

Parameters
afecBase address of the AFEC.
Returns
The interrupt status value.

Referenced by afec_init(), and afec_process_callback().

static uint32_t afec_get_latest_chan_num ( Afec *const  afec)
inlinestatic

Get the Last Converted Channel Number.

Parameters
afecBase address of the AFEC.
Returns
AFEC Last Converted Channel Number.
static uint32_t afec_get_latest_value ( Afec *const  afec)
inlinestatic

Get the Last Data Converted.

Parameters
afecBase address of the AFEC.
Returns
AFEC latest converted value.
static uint32_t afec_get_overrun_status ( Afec *const  afec)
inlinestatic

Get AFEC overrun error status.

Parameters
afecBase address of the AFEC.
Returns
AFEC overrun error status.
static uint32_t afec_get_writeprotect_status ( Afec *const  afec)
inlinestatic

Indicate write protect status.

Parameters
afecBase address of the AFEC.
Returns
0 if no write protect violation occurred, or 16-bit write protect violation source.
static void afec_set_comparison_window ( Afec *const  afec,
const uint16_t  us_low_threshold,
const uint16_t  us_high_threshold 
)
inlinestatic

Configure AFEC compare window.

Parameters
afecBase address of the AFEC.
us_low_thresholdLow threshold of compare window.
us_high_thresholdHigh threshold of compare window.
static void afec_set_resolution ( Afec *const  afec,
const enum afec_resolution  res 
)
inlinestatic

Configure conversion resolution.

Parameters
afecBase address of the AFEC.
resConversion resolution.
static void afec_set_trigger ( Afec *const  afec,
const enum afec_trigger  trigger 
)
inlinestatic

Configure conversion trigger and free run mode.

Parameters
afecBase address of the AFEC.
triggerConversion trigger.

References AFEC_TRIG_FREERUN.

Referenced by main().

static void afec_set_writeprotect ( Afec *const  afec,
const bool  is_enable 
)
inlinestatic

Enable or disable write protection of AFEC registers.

Parameters
afecBase address of the AFEC.
is_enable1 to enable, 0 to disable.
static void afec_start_software_conversion ( Afec *const  afec)
inlinestatic

Start analog-to-digital conversion.

Note
If one of the hardware event is selected as AFEC trigger, this function can NOT start analog to digital conversion.
Parameters
afecBase address of the AFEC.