This is the unit test application for the AFEC driver. It consists of test cases for the following functionality:
The SAM4E ,SAMV71-Xplained-Ultra ,SAME70-Xplained-Pro devices can be used.
This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/