This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Direct Memory Access DMA Controller (DMAC) functionality.
The DMAC is an AHB-central DMA controller core that transfers data from a source peripheral to a destination peripheral over one or more AMBA buses. This is a driver for the configuration, enabling, disabling, and use of the DMAC peripheral.
Devices from the following series can use this module:
The outline of this documentation is as follows:
There are no prerequisites for this module.
The DMA Controller (DMAC) is an AHB-central DMA controller core that transfers data from a source peripheral to a destination peripheral over one or more AMBA buses. One channel is required for each source/destination pair. In the most basic configuration, the DMAC has one master interface and one channel. The master interface reads the data from a source and writes it to a destination. Two AMBA transfers are required for each DMAC data transfer. This is also known as a dual-access transfer.
There are no special considerations for this module.
For extra information, see Extra Information for Direct Memory Access Controller Driver. This includes:
For a list of examples related to this driver, see Examples for Direct Memory Access Controller Driver.
Data Structures | |
struct | dma_transfer_descriptor_t |
DMA transfer descriptor structure, otherwise known as a Linked List Item (LLI). More... | |
Enumerations | |
enum | dmac_priority_mode_t { DMAC_PRIORITY_FIXED = 0, DMAC_PRIORITY_ROUND_ROBIN = DMAC_GCFG_ARB_CFG } |
DMAC priority mode. More... | |
Functions | |
void | dmac_channel_disable (Dmac *p_dmac, uint32_t ul_num) |
Disable the specified DMA Channel. More... | |
void | dmac_channel_enable (Dmac *p_dmac, uint32_t ul_num) |
Enable the specified DMA Channel. More... | |
uint32_t | dmac_channel_get_status (Dmac *p_dmac) |
Get the DMAC Channel handler status. More... | |
uint32_t | dmac_channel_is_enable (Dmac *p_dmac, uint32_t ul_num) |
Check if the specified DMA Channel is enabled. More... | |
uint32_t | dmac_channel_is_transfer_done (Dmac *p_dmac, uint32_t ul_num) |
Check if the data transfer occurring on the specified DMA Channel is complete. More... | |
void | dmac_channel_keep (Dmac *p_dmac, uint32_t ul_num) |
Resume the specified DMA Channel from an automatic stall state. More... | |
void | dmac_channel_multi_buf_transfer_init (Dmac *p_dmac, uint32_t ul_num, dma_transfer_descriptor_t *p_desc) |
Initialize the DMA Channel for a multiple buffer transfer. More... | |
void | dmac_channel_resume (Dmac *p_dmac, uint32_t ul_num) |
Resume the specified DMA Channel transfer (restoring its context). More... | |
void | dmac_channel_set_configuration (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_cfg) |
Set the DMAC configuration register of the specified DMA Channel. More... | |
void | dmac_channel_set_ctrlA (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_ctrlA) |
Set the DMA control A of the specified DMA Channel. More... | |
void | dmac_channel_set_ctrlB (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_ctrlB) |
Set the DMA control B of the specified DMA Channel. More... | |
void | dmac_channel_set_descriptor_addr (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_desc) |
Set the DMA descriptor address of the specified DMA Channel. More... | |
void | dmac_channel_set_destination_addr (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_addr) |
Set the DMA destination address of the specified DMA Channel. More... | |
void | dmac_channel_set_source_addr (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_addr) |
Set the DMA source address of the specified DMA Channel. More... | |
void | dmac_channel_single_buf_transfer_init (Dmac *p_dmac, uint32_t ul_num, dma_transfer_descriptor_t *p_desc) |
Initialize the DMA Channel for a single buffer transfer. More... | |
void | dmac_channel_stop_transfer (Dmac *p_dmac, uint32_t ul_num) |
Stop a DMA transfer occurring on the specified DMA Channel. More... | |
void | dmac_channel_suspend (Dmac *p_dmac, uint32_t ul_num) |
Suspend the specified DMA Channel and its current context. More... | |
void | dmac_disable (Dmac *p_dmac) |
Disable the DMA Controller. More... | |
void | dmac_disable_interrupt (Dmac *p_dmac, uint32_t ul_mask) |
Disable DMAC interrupts. More... | |
void | dmac_enable (Dmac *p_dmac) |
Enable the DMA Controller. More... | |
void | dmac_enable_interrupt (Dmac *p_dmac, uint32_t ul_mask) |
Enable DMAC interrupts. More... | |
uint32_t | dmac_get_interrupt_mask (Dmac *p_dmac) |
Get the DMAC Interrupt Mask. More... | |
uint32_t | dmac_get_status (Dmac *p_dmac) |
Get the DMAC transfer status. More... | |
void | dmac_init (Dmac *p_dmac) |
Initialize the DMA controller and disable it. More... | |
void | dmac_set_priority_mode (Dmac *p_dmac, dmac_priority_mode_t mode) |
Set the DMA priority mode. More... | |
void | dmac_soft_chunk_transfer_request (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_src_req, uint32_t ul_dst_req) |
DMA Channel software chunk request. More... | |
void | dmac_soft_set_last_transfer_flag (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_src_flag, uint32_t ul_dst_flag) |
Set the DMA Channel's last transfer flag. More... | |
void | dmac_soft_single_transfer_request (Dmac *p_dmac, uint32_t ul_num, uint32_t ul_src_req, uint32_t ul_dst_req) |
DMA Channel software single request. More... | |
enum dmac_priority_mode_t |
void dmac_channel_disable | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Disable the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
References Assert.
Referenced by dmac_channel_stop_transfer().
void dmac_channel_enable | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Enable the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
References Assert.
Referenced by run_multi_buf_xfer_test(), and run_single_buf_xfer_test().
uint32_t dmac_channel_get_status | ( | Dmac * | p_dmac | ) |
Get the DMAC Channel handler status.
[in] | p_dmac | Module hardware register base address pointer |
References Assert.
Referenced by dmac_channel_is_transfer_done(), and dmac_channel_stop_transfer().
uint32_t dmac_channel_is_enable | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Check if the specified DMA Channel is enabled.
[in] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
0 | DMA Channel is disabled |
1 | DMA Channel is enabled |
References Assert.
uint32_t dmac_channel_is_transfer_done | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Check if the data transfer occurring on the specified DMA Channel is complete.
[in] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
0 | Data is transferring |
1 | Data transfer complete |
References Assert, and dmac_channel_get_status().
Referenced by run_single_buf_xfer_test().
void dmac_channel_keep | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Resume the specified DMA Channel from an automatic stall state.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
References Assert.
void dmac_channel_multi_buf_transfer_init | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
dma_transfer_descriptor_t * | p_desc | ||
) |
Initialize the DMA Channel for a multiple buffer transfer.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | p_desc | Pointer to a transfer descriptor |
References Assert, dmac_channel_set_ctrlB(), and dmac_channel_set_descriptor_addr().
Referenced by run_multi_buf_xfer_test().
void dmac_channel_resume | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Resume the specified DMA Channel transfer (restoring its context).
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
References Assert.
Referenced by dmac_channel_stop_transfer().
void dmac_channel_set_configuration | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_cfg | ||
) |
Set the DMAC configuration register of the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_cfg | Configuration of CFG register |
References Assert.
Referenced by run_multi_buf_xfer_test(), and run_single_buf_xfer_test().
void dmac_channel_set_ctrlA | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_ctrlA | ||
) |
Set the DMA control A of the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_ctrlA | Configuration of control A register |
References Assert.
Referenced by dmac_channel_single_buf_transfer_init().
void dmac_channel_set_ctrlB | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_ctrlB | ||
) |
Set the DMA control B of the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_ctrlB | Configuration of control B register |
References Assert.
Referenced by dmac_channel_multi_buf_transfer_init(), and dmac_channel_single_buf_transfer_init().
void dmac_channel_set_descriptor_addr | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_desc | ||
) |
Set the DMA descriptor address of the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_desc | Descriptor address |
References Assert.
Referenced by dmac_channel_multi_buf_transfer_init(), and dmac_channel_single_buf_transfer_init().
void dmac_channel_set_destination_addr | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_addr | ||
) |
Set the DMA destination address of the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_addr | Destination address |
References Assert.
Referenced by dmac_channel_single_buf_transfer_init().
void dmac_channel_set_source_addr | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_addr | ||
) |
Set the DMA source address of the specified DMA Channel.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_addr | Source address |
References Assert.
Referenced by dmac_channel_single_buf_transfer_init().
void dmac_channel_single_buf_transfer_init | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
dma_transfer_descriptor_t * | p_desc | ||
) |
Initialize the DMA Channel for a single buffer transfer.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | p_desc | Pointer to a transfer descriptor |
References Assert, dmac_channel_set_ctrlA(), dmac_channel_set_ctrlB(), dmac_channel_set_descriptor_addr(), dmac_channel_set_destination_addr(), dmac_channel_set_source_addr(), dma_transfer_descriptor_t::ul_ctrlA, dma_transfer_descriptor_t::ul_ctrlB, dma_transfer_descriptor_t::ul_destination_addr, and dma_transfer_descriptor_t::ul_source_addr.
Referenced by run_single_buf_xfer_test().
void dmac_channel_stop_transfer | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Stop a DMA transfer occurring on the specified DMA Channel.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
References Assert, dmac_channel_disable(), dmac_channel_get_status(), dmac_channel_resume(), and dmac_channel_suspend().
void dmac_channel_suspend | ( | Dmac * | p_dmac, |
uint32_t | ul_num | ||
) |
Suspend the specified DMA Channel and its current context.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
References Assert.
Referenced by dmac_channel_stop_transfer().
void dmac_disable | ( | Dmac * | p_dmac | ) |
Disable the DMA Controller.
[in,out] | p_dmac | Module hardware register base address pointer |
References Assert.
Referenced by dmac_init().
void dmac_disable_interrupt | ( | Dmac * | p_dmac, |
uint32_t | ul_mask | ||
) |
Disable DMAC interrupts.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_mask | A bitmask of interrupts to be disabled |
Where input parameter ul_mask is a bitmask containing one or more of the following:
Parameter Value | Description |
---|---|
DMAC_EBCIDR_BTC0 | Channel 0 Buffer Transfer Completed |
DMAC_EBCIDR_BTC1 | Channel 1 Buffer Transfer Completed |
DMAC_EBCIDR_BTC2 | Channel 2 Buffer Transfer Completed |
DMAC_EBCIDR_BTC3 | Channel 3 Buffer Transfer Completed |
DMAC_EBCIDR_CBTC0 | Channel 0 Chained Buffer Transfer Completed |
DMAC_EBCIDR_CBTC1 | Channel 1 Chained Buffer Transfer Completed |
DMAC_EBCIDR_CBTC2 | Channel 2 Chained Buffer Transfer Completed |
DMAC_EBCIDR_CBTC3 | Channel 3 Chained Buffer Transfer Completed |
DMAC_EBCIDR_ERR0 | Channel 0 Access Error |
DMAC_EBCIDR_ERR1 | Channel 1 Access Error |
DMAC_EBCIDR_ERR2 | Channel 2 Access Error |
DMAC_EBCIDR_ERR3 | Channel 3 Access Error |
References Assert.
void dmac_enable | ( | Dmac * | p_dmac | ) |
Enable the DMA Controller.
[out] | p_dmac | Module hardware register base address pointer |
References Assert.
Referenced by run_multi_buf_xfer_test(), and run_single_buf_xfer_test().
void dmac_enable_interrupt | ( | Dmac * | p_dmac, |
uint32_t | ul_mask | ||
) |
Enable DMAC interrupts.
[out] | p_dmac | Module hardware register base address pointer |
[in] | ul_mask | A bitmask of interrupts to be enabled |
Where input parameter ul_mask is a bitmask containing one or more of the following:
Parameter Value | Description |
---|---|
DMAC_EBCIER_BTC0 | Channel 0 Buffer Transfer Completed |
DMAC_EBCIER_BTC1 | Channel 1 Buffer Transfer Completed |
DMAC_EBCIER_BTC2 | Channel 2 Buffer Transfer Completed |
DMAC_EBCIER_BTC3 | Channel 3 Buffer Transfer Completed |
DMAC_EBCIER_CBTC0 | Channel 0 Chained Buffer Transfer Completed |
DMAC_EBCIER_CBTC1 | Channel 1 Chained Buffer Transfer Completed |
DMAC_EBCIER_CBTC2 | Channel 2 Chained Buffer Transfer Completed |
DMAC_EBCIER_CBTC3 | Channel 3 Chained Buffer Transfer Completed |
DMAC_EBCIER_ERR0 | Channel 0 Access Error |
DMAC_EBCIER_ERR1 | Channel 1 Access Error |
DMAC_EBCIER_ERR2 | Channel 2 Access Error |
DMAC_EBCIER_ERR3 | Channel 3 Access Error |
References Assert.
Referenced by run_multi_buf_xfer_test().
uint32_t dmac_get_interrupt_mask | ( | Dmac * | p_dmac | ) |
Get the DMAC Interrupt Mask.
[in] | p_dmac | Module hardware register base address pointer |
References Assert.
uint32_t dmac_get_status | ( | Dmac * | p_dmac | ) |
Get the DMAC transfer status.
[in] | p_dmac | Module hardware register base address pointer |
References Assert.
Referenced by DMAC_Handler().
void dmac_init | ( | Dmac * | p_dmac | ) |
Initialize the DMA controller and disable it.
[in,out] | p_dmac | Module hardware register base address pointer |
References dmac_disable().
Referenced by run_multi_buf_xfer_test(), and run_single_buf_xfer_test().
void dmac_set_priority_mode | ( | Dmac * | p_dmac, |
dmac_priority_mode_t | mode | ||
) |
Set the DMA priority mode.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | mode | Priority mode |
References Assert.
Referenced by run_multi_buf_xfer_test(), and run_single_buf_xfer_test().
void dmac_soft_chunk_transfer_request | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_src_req, | ||
uint32_t | ul_dst_req | ||
) |
DMA Channel software chunk request.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_src_req | Request a source transfer |
[in] | ul_dst_req | Request a destination transfer |
References Assert.
void dmac_soft_set_last_transfer_flag | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_src_flag, | ||
uint32_t | ul_dst_flag | ||
) |
Set the DMA Channel's last transfer flag.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | Channel number |
[in] | ul_src_flag | Last source transfer flag |
[in] | ul_dst_flag | Last destination transfer flag |
References Assert.
void dmac_soft_single_transfer_request | ( | Dmac * | p_dmac, |
uint32_t | ul_num, | ||
uint32_t | ul_src_req, | ||
uint32_t | ul_dst_req | ||
) |
DMA Channel software single request.
[in,out] | p_dmac | Module hardware register base address pointer |
[in] | ul_num | DMA Channel number (range 0 to 3) |
[in] | ul_src_req | Request a source transfer |
[in] | ul_dst_req | Request a destination transfer |
References Assert.