This module is the test suite framework, which provides a set of standard functions and macros for defining and running test suites.
A test suite consists of test cases. Each test case consists of a set of functions that are called in a specific order by the framework when the test suite is run. The runtime environment of a test is referred to as the test fixture. A setup function can be defined for the purpose of fulfilling preconditions that are needed for the test to run. To free up or reset resources which were used in the test case, a cleanup function can be defined.
The following three functions can be defined for each test case:
The setup and/or cleanup functions may be skipped if they are not needed.
A function may report an error or failure by use of the macros test_fail , test_assert_true and test_assert_false. Note that only the first macro allows for the result value to be specified, while the two latter will automatically return TEST_FAIL if the specified condition is false.
If any of the functions return a failure/error result, execution of that specific function is ended. However, depending on which function did not pass, execution of the test case may continue:
The result of the first function in the test case which does not pass determines the end result.
Example code for definition of a test suite:
Example code for definition of a test case:
Data Structures | |
struct | test_case |
A test case. More... | |
struct | test_suite |
A test suite. More... | |
Functions | |
static int | test_call (void(*func)(const struct test_case *), const struct test_case *test) |
Call a test or fixture function. More... | |
void | test_case_fail (const struct test_case *test, int result, const char *file, unsigned int line, const char *fmt,...) |
Report a failure and jump out of current test case function. More... | |
static int | test_case_run (const struct test_case *test) |
Run a test case. More... | |
static void | test_report_failure (const struct test_case *test, const char *stage, int result) |
Report a failing test stage. More... | |
Variables | |
struct test_case * | test_case_ptr = NULL |
Pointer to current test case. More... | |
static jmp_buf | test_failure_jmpbuf |
Context saved before executing a test or fixture function. More... | |
void * | test_priv_data |
Data pointer for test cases. More... | |
Wrappers for printing debug information | |
| |
#define | dbg(__fmt_) printf_P(PROGMEM_STRING(__fmt_)) |
#define | dbg_info(__fmt_,...) printf_P(PROGMEM_STRING(__fmt_), __VA_ARGS__) |
#define | dbg_error(_x,...) printf_P(PROGMEM_STRING(_x), __VA_ARGS__) |
#define | dbg_putchar(c) putc(c, stdout) |
#define | dbg_vprintf_pgm(...) vfprintf_P(stdout, __VA_ARGS__) |
Test suite definition macros | |
#define | DEFINE_TEST_CASE(_sym, _setup, _run, _cleanup, _name) |
Create a test case struct. More... | |
#define | DEFINE_TEST_ARRAY(_sym) const struct test_case *const _sym[] |
Create an array of test case pointers. More... | |
#define | DEFINE_TEST_SUITE(_sym, _test_array, _name) |
Create a test suite. More... | |
Test data access | |
void * | test_priv_data |
Data pointer for test cases. More... | |
static void | test_set_data (void *data) |
Set private data pointer for the current test. More... | |
static void * | test_get_data (void) |
Get the private data pointer for the current test. More... | |
Test case pointer access | |
struct test_case * | test_case_ptr |
Pointer to current test case. More... | |
static void | test_set_case (const struct test_case *test) |
Set pointer to current test. More... | |
static struct test_case * | test_get_case (void) |
Get pointer to current test. More... | |
Test result reporting | |
enum | test_status { TEST_ERROR = -1, TEST_PASS = 0, TEST_FAIL = 1 } |
Status codes returned by test cases and fixtures. More... | |
#define | test_fail(test, result,...) test_case_fail(test, result, __FILE__, __LINE__, __VA_ARGS__) |
Fail the test. More... | |
#define | test_assert_true(test, condition,...) |
Verify that condition is true. More... | |
#define | test_assert_false(test, condition,...) test_assert_true(test, !(condition), __VA_ARGS__) |
Verify that condition is false. More... | |
Test suite interaction | |
int | test_suite_run (const struct test_suite *suite) |
Run a test suite. More... | |
#define dbg | ( | __fmt_ | ) | printf_P(PROGMEM_STRING(__fmt_)) |
Referenced by test_case_run().
#define dbg_error | ( | _x, | |
... | |||
) | printf_P(PROGMEM_STRING(_x), __VA_ARGS__) |
Referenced by test_case_fail(), and test_report_failure().
#define dbg_info | ( | __fmt_, | |
... | |||
) | printf_P(PROGMEM_STRING(__fmt_), __VA_ARGS__) |
Referenced by test_case_run(), and test_suite_run().
#define dbg_putchar | ( | c | ) | putc(c, stdout) |
Referenced by test_case_fail().
#define dbg_vprintf_pgm | ( | ... | ) | vfprintf_P(stdout, __VA_ARGS__) |
Referenced by test_case_fail().
#define DEFINE_TEST_ARRAY | ( | _sym | ) | const struct test_case *const _sym[] |
Create an array of test case pointers.
_sym | Variable name of the resulting array |
Referenced by main().
#define DEFINE_TEST_CASE | ( | _sym, | |
_setup, | |||
_run, | |||
_cleanup, | |||
_name | |||
) |
Create a test case struct.
_sym | Variable name of the resulting struct |
_setup | Function which sets up a test case environment. Can be NULL. |
_run | Test function |
_cleanup | Function which cleans up what was set up. Can be NULL. |
_name | String describing the test case. |
Referenced by main().
#define DEFINE_TEST_SUITE | ( | _sym, | |
_test_array, | |||
_name | |||
) |
Create a test suite.
_sym | Variable name of the resulting struct |
_test_array | Array of test cases, created with DEFINE_TEST_ARRAY() |
_name | String describing the test suite. |
Referenced by main().
#define test_assert_false | ( | test, | |
condition, | |||
... | |||
) | test_assert_true(test, !(condition), __VA_ARGS__) |
Verify that condition is false.
If condition is true, fail the test with an error message indicating the condition which failed.
test | The test case currently being run |
condition | Expression to be validated |
... | Format string and arguments |
#define test_assert_true | ( | test, | |
condition, | |||
... | |||
) |
Verify that condition is true.
If condition is false, fail the test with an error message indicating the condition which failed.
test | The test case currently being run |
condition | Expression to be validated |
... | Format string and arguments |
Referenced by run_eic_test().
#define test_fail | ( | test, | |
result, | |||
... | |||
) | test_case_fail(test, result, __FILE__, __LINE__, __VA_ARGS__) |
Fail the test.
Calling this function will cause the test to terminate with a failure. It will return directly to the test suite core, not to the caller.
test | Test case which failed |
result | The result of the test (may not be 0) |
... | printf()-style format string and arguments |
enum test_status |
Status codes returned by test cases and fixtures.
Note that test cases and especially fixtures may return any of the status codes defined by status_code as well.
Enumerator | |
---|---|
TEST_ERROR |
Test error. |
TEST_PASS |
Test success. |
TEST_FAIL |
Test failure. |
|
static |
Call a test or fixture function.
This function will initialize test_failure_jmpbuf and call func with test as the parameter.
func | Pointer to function to call. |
test_case | Pointer to the function's originating test case. |
References test_failure_jmpbuf, and TEST_PASS.
Referenced by test_case_run().
void test_case_fail | ( | const struct test_case * | test, |
int | result, | ||
const char * | file, | ||
unsigned int | line, | ||
const char * | fmt, | ||
... | |||
) |
Report a failure and jump out of current test case function.
test | Current test case. |
result | Result value of failure. |
file | Name of file in which function resides. |
line | Line number at which failure occurred. |
fmt | Failure message, as printf-formatted string. |
... | Values to insert into failure message. |
References dbg_error, dbg_putchar, dbg_vprintf_pgm, test_case::name, and test_failure_jmpbuf.
|
static |
Run a test case.
This function will call the setup, run and cleanup functions of the specified test case, outputting debug information as it goes, then returning the result value of the test case.
If the setup stage does not pass, the rest of the test case if skipped. If the test stage itself does not pass, the cleanup is still executed.
The result from the first non-passing function in the test case is returned, meaning a failing cleanup will override a successful test.
test_case | Test case to run. |
References test_case::cleanup, dbg, dbg_info, test_case::name, test_case::run, test_case::setup, test_call(), test_report_failure(), and test_set_case().
Referenced by test_suite_run().
|
static |
Get pointer to current test.
References test_case_ptr.
|
inlinestatic |
Get the private data pointer for the current test.
References test_priv_data.
|
static |
Report a failing test stage.
test | Current test case. |
stage | Name of test stage that failed. |
result | Result value of test stage. |
References dbg_error, and test_case::name.
Referenced by test_case_run().
|
inlinestatic |
Set pointer to current test.
Referenced by test_case_run().
|
inlinestatic |
Set private data pointer for the current test.
data | Pointer to arbitrary run-time data for the test currently being run. |
References test_priv_data.
int test_suite_run | ( | const struct test_suite * | suite | ) |
Run a test suite.
Run all tests in suite, in the order in which they are found in the array.
References dbg_info, test_suite::name, test_suite::nr_tests, test_case_run(), TEST_PASS, and test_suite::tests.
Referenced by main().
struct test_case* test_case_ptr = NULL |
Pointer to current test case.
Referenced by test_get_case().
struct test_case* test_case_ptr |
Pointer to current test case.
Referenced by test_get_case().
|
static |
Context saved before executing a test or fixture function.
This is used for doing non-local jumps from the test cases on failure.
Referenced by test_call(), and test_case_fail().
void* test_priv_data |
Data pointer for test cases.
Referenced by test_get_data(), and test_set_data().
void* test_priv_data |
Data pointer for test cases.
Referenced by test_get_data(), and test_set_data().