Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
PEVC Unit Test for SAM4L Xplained Pro Documentation

Introduction

This is the unit test application for Events driver (PEVC). It consists of test cases for the following functionality:

  • Using the AST as an event source and the DACC as a triggered event.
  • Using the software trigger as an event source and the DACC as a triggered event.

Main Files

Device Info

SAM4L devices can be used. This example has been tested with the following setup:

  • sam4l4c_sam4l_ek
  • sam4lc4c_sam4l_xplained_pro
  • sam4lc8c_sam4l8_xplained_pro

Compilation info

This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.

Contact Information

For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/