This is the documentation for the data structures, functions, variables, defines, enums, and typedefs for the FLASHCALW software driver.
The example2 demonstrates how to read the unique ID of a SAM4L device.
Operating mode of the example:
This software is written for GNU GCC and IAR Embedded Workbench for Atmel. Other compilers may or may not work.
All SAM devices with a FLASHCALW module can be used.
This example has been tested with the following kits:
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/