Microchip® Advanced Software Framework

flashcalw_example3.c File Reference

FLASHCALW example3 for SAM.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "time_tick.h"

Macros

#define FIBONACCI_NUM   32
 Fibonacci number. More...
 
#define LOWER_SYS_CLK   12000000
 

Functions

static void configure_console (void)
 Configure serial console. More...
 
static void flash_picocache_example (const char *caption, bool pico_enable)
 This is an example demonstrating Fibonacci calculation with and without PicoCache. More...
 
int main (void)
 main function. More...
 
static uint32_t recfibo (uint32_t n)
 Recursively calculate the nth Fibonacci number. More...
 
static void reconfigure_com_port (void)
 Reconfigure serial console. More...
 
static void wait_for_pushbutton (void)
 

#define FIBONACCI_NUM   32

Fibonacci number.

Referenced by flash_picocache_example().

#define LOWER_SYS_CLK   12000000

Referenced by reconfigure_com_port().

static void configure_console ( void  )
static
static void flash_picocache_example ( const char *  caption,
bool  pico_enable 
)
static

This is an example demonstrating Fibonacci calculation with and without PicoCache.

Parameters
captionCaption to print before running the example.
pico_enableEnable PicoCache or not.

References FIBONACCI_NUM, flashcalw_picocache_disable(), flashcalw_picocache_disable_monitor(), flashcalw_picocache_enable(), flashcalw_picocache_enable_monitor(), flashcalw_picocache_get_monitor_cnt(), flashcalw_picocache_reset_monitor(), flashcalw_picocache_set_monitor_mode(), recfibo(), time_tick_calc_delay(), and time_tick_get().

Referenced by main().

int main ( void  )

main function.

Do the Fibonacci calculation with and without PicoCache and print the calculation time to the UART console.

References board_init(), BOARD_NAME, BUTTON_0_NAME, configure_console(), flash_picocache_example(), flashcalw_set_wait_state(), reconfigure_com_port(), sysclk_get_cpu_hz(), sysclk_init(), sysclk_set_prescalers(), time_tick_init(), and wait_for_pushbutton().

static uint32_t recfibo ( uint32_t  n)
static

Recursively calculate the nth Fibonacci number.

Parameters
nIndicates which (positive) Fibonacci number to compute.
Returns
The nth Fibonacci number.

Referenced by flash_picocache_example().

static void reconfigure_com_port ( void  )
static
static void wait_for_pushbutton ( void  )
static

References delay_ms, GPIO_PUSH_BUTTON_0, and ioport_get_pin_level().

Referenced by main().