Configuration File for GPIO example.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | EXAMPLE_BUTTON_INT GPIO_PUSH_BUTTON_0 |
Using button PB0 on SAM4L-EK to trigger an interrupt. More... | |
#define | EXAMPLE_GND_NAME "J4/PIN9" |
#define | EXAMPLE_LED LED0 |
#define | EXAMPLE_PIN_EVENT PIN_PC08 |
Using PC08 on SAM4L-EK to trigger an event. More... | |
#define | EXAMPLE_PIN_NAME "PC08" |
#define | PDCA_PID_USART_TX 20 |
PDCA ID for USART TX. More... | |
#define EXAMPLE_BUTTON_INT GPIO_PUSH_BUTTON_0 |
Using button PB0 on SAM4L-EK to trigger an interrupt.
Referenced by main().
#define EXAMPLE_GND_NAME "J4/PIN9" |
Referenced by main().
#define EXAMPLE_LED LED0 |
#define EXAMPLE_PIN_EVENT PIN_PC08 |
Using PC08 on SAM4L-EK to trigger an event.
Referenced by main().
#define EXAMPLE_PIN_NAME "PC08" |
Referenced by main().
#define PDCA_PID_USART_TX 20 |
PDCA ID for USART TX.
Referenced by init_pdca().