HMATRIX driver for SAM.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
Data Structures | |
struct | hmatrix_master_ch_conf |
HMatrix Master Channel configuration structure. More... | |
struct | hmatrix_slave_ch_conf |
HMatrix Slave Channel configuration structure. More... | |
Macros | |
#define | hmatrix_prs HmatrixbPrs |
Enumerations | |
enum | hmatrix_arbitration_type { HMATRIX_ARBITRATION_ROUND_ROBIN = HMATRIXB_SCFG_ARBT_ROUND_ROBIN, HMATRIX_ARBITRATION_FIXED_PRIORITY = HMATRIXB_SCFG_ARBT_FIXED_PRIORITY } |
HMATRIX slave: arbitration type. More... | |
enum | hmatrix_burst_type { HMATRIX_BURST_INFINITE_LENGTH = HMATRIXB_MCFG_ULBT(0), HMATRIX_BURST_SINGLE_ACCESS = HMATRIXB_MCFG_ULBT(1), HMATRIX_BURST_FOUR_BEAT = HMATRIXB_MCFG_ULBT(2), HMATRIX_BURST_EIGHT_BEAT = HMATRIXB_MCFG_ULBT(3), HMATRIX_BURST_SIXTEEN_BEAT = HMATRIXB_MCFG_ULBT(4) } |
HMATRIX master: undefined length burst type. More... | |
enum | hmatrix_def_master_type { HMATRIX_DEFAULT_MASTER_NONE = HMATRIXB_SCFG_DEFMSTR_TYPE(0), HMATRIX_DEFAULT_MASTER_PREVIOUS = HMATRIXB_SCFG_DEFMSTR_TYPE(1), HMATRIX_DEFAULT_MASTER_FIXED = HMATRIXB_SCFG_DEFMSTR_TYPE(2) } |
HMATRIX slave: default master type. More... | |
enum | hmatrix_master_id { HMATRIX_MASTER_ID_CPU_IDCORE = HMATRIX_MASTER_CPU_IDCODE, HMATRIX_MASTER_ID_CPU_SYS = HMATRIX_MASTER_CPU_SYS, HMATRIX_MASTER_ID_SMAP = HMATRIX_MASTER_SMAP, HMATRIX_MASTER_ID_PDC = HMATRIX_MASTER_PDCA, HMATRIX_MASTER_ID_USB = HMATRIX_MASTER_USBC_MASTER, HMATRIX_MASTER_ID_CRCCU = HMATRIX_MASTER_CRCCU, HMATRIX_MASTER_ID_NUM } |
Master identifier. More... | |
enum | hmatrix_slave_id { HMATRIX_SLAVE_ID_FLASH = HMATRIX_SLAVE_FLASH, HMATRIX_SLAVE_ID_PBA = HMATRIX_SLAVE_HTOP0, HMATRIX_SLAVE_ID_PBB = HMATRIX_SLAVE_HTOP1, HMATRIX_SLAVE_ID_PBC = HMATRIX_SLAVE_HTOP2, HMATRIX_SLAVE_ID_PBD = HMATRIX_SLAVE_HTOP3, HMATRIX_SLAVE_ID_HRAMC0 = HMATRIX_SLAVE_HRAMC0, HMATRIX_SLAVE_ID_HRAMC1 = HMATRIX_SLAVE_HRAMC1, HMATRIX_SLAVE_ID_AES = HMATRIX_SLAVE_AESA, HMATRIX_SLAVE_ID_NUM } |
Slave identifier. More... | |
Functions | |
void | hmatrix_disable (void) |
Disables the HMatrix. More... | |
void | hmatrix_enable (void) |
Enables the HMatrix. More... | |
void | hmatrix_get_slave_priority (enum hmatrix_slave_id slave_id, hmatrix_prs *p_prio) |
Get priority for the specified slave access. More... | |
void | hmatrix_init (void) |
Initializes the HMatrix. More... | |
static void | hmatrix_master_ch_get_config_defaults (struct hmatrix_master_ch_conf *const config) |
Initializes an HMatrix Master configuration structure to defaults. More... | |
void | hmatrix_master_ch_set_config (const enum hmatrix_master_id master_id, struct hmatrix_master_ch_conf *const config) |
Writes an HMatrix Master channel configuration to the hardware module. More... | |
void | hmatrix_set_slave_priority (enum hmatrix_slave_id slave_id, hmatrix_prs *p_prio) |
Set priority for the specified slave access. More... | |
static void | hmatrix_slave_ch_get_config_defaults (struct hmatrix_slave_ch_conf *const config) |
Initializes an HMatrix Slave configuration structure to defaults. More... | |
void | hmatrix_slave_ch_set_config (const enum hmatrix_slave_id slave_id, struct hmatrix_slave_ch_conf *const config) |
Writes an HMatrix Slave channel configuration to the hardware module. More... | |
#define hmatrix_prs HmatrixbPrs |
enum hmatrix_burst_type |
enum hmatrix_master_id |
enum hmatrix_slave_id |
|
inlinestatic |
Initializes an HMatrix Master configuration structure to defaults.
Initializes a given HMatrix Master channel configuration structure to a set of known default values. This function should be called on all new instances of these configuration structures before being modified by the user application.
The default configuration is as follows:
config | Configuration structure to initialize to default values |
References Assert, hmatrix_master_ch_conf::burst_type, and HMATRIX_BURST_FOUR_BEAT.
|
inlinestatic |
Initializes an HMatrix Slave configuration structure to defaults.
Initializes a given HMatrix Slave channel configuration structure to a set of known default values. This function should be called on all new instances of these configuration structures before being modified by the user application.
The default configuration is as follows:
config | Configuration structure to initialize to default values |
References hmatrix_slave_ch_conf::arbitration_type, Assert, hmatrix_slave_ch_conf::def_master_type, hmatrix_slave_ch_conf::fixed_def_master_number, HMATRIX_ARBITRATION_ROUND_ROBIN, HMATRIX_DEFAULT_MASTER_PREVIOUS, HMATRIX_MASTER_ID_CPU_IDCORE, and hmatrix_slave_ch_conf::slot_cycle.
Referenced by main().