ICM region descriptor in secondary list.
#include <icm.h>
Data Fields | |
struct icm_region_descriptor_sec_list * | next_addr |
The address of next region descriptor in secondary list. More... | |
uint32_t | reserved |
uint32_t | start_addr |
The first byte address of the region. More... | |
uint32_t | tran_size |
The number of blocks(512 bits) transferred from the memory to the SHA engine. More... | |
struct icm_region_descriptor_sec_list* icm_region_descriptor_sec_list::next_addr |
The address of next region descriptor in secondary list.
uint32_t icm_region_descriptor_sec_list::reserved |
uint32_t icm_region_descriptor_sec_list::start_addr |
The first byte address of the region.
uint32_t icm_region_descriptor_sec_list::tran_size |
The number of blocks(512 bits) transferred from the memory to the SHA engine.
Transfer size = (tran_size + 1) * 512bits The maxium size is 65536.