This is the unit test application for the PICOUART driver. It requires a board monitor firmware version V1.3 or greater. It contains one test case for the PICOUART module:
SAM4L devices can be used. This example has been tested with the following setup:
This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/