This is the unit test application for the PWM driver. It consists of test cases for the following functionality:
All SAM devices can be used. This example has been tested with the following setup:
This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.
For further information, visit Microchip.
Support and FAQ: https://www.microchip.com/support/