Real-time Timer (RTT) example for SAM.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ASCII_BS 8 |
ASCII char definition for backspace. More... | |
#define | ASCII_CR 13 |
ASCII char definition for carriage return. More... | |
#define | STATE_MAIN_MENU 0 |
Device state: in the main menu. More... | |
#define | STATE_SET_ALARM 1 |
Device state: user is setting an alarm time. More... | |
#define | STRING_EOL "\r" |
#define | STRING_HEADER |
Functions | |
static void | configure_console (void) |
Configure the console UART. More... | |
static void | configure_rtt (void) |
RTT configuration function. More... | |
int | main (void) |
Application entry point for RTT example. More... | |
static void | refresh_display (void) |
Refresh display on terminal. More... | |
void | RTT_Handler (void) |
Interrupt handler for the RTT. More... | |
Variables | |
volatile uint8_t | g_uc_alarmed |
Indicate that an alarm has occurred but has not been cleared. More... | |
volatile uint8_t | g_uc_state |
Current device state. More... | |
volatile uint32_t | g_ul_new_alarm |
New alarm time being currently entered. More... | |
#define ASCII_BS 8 |
ASCII char definition for backspace.
Referenced by main().
#define ASCII_CR 13 |
ASCII char definition for carriage return.
Referenced by main().
#define STATE_MAIN_MENU 0 |
Device state: in the main menu.
Referenced by main(), and refresh_display().
#define STATE_SET_ALARM 1 |
Device state: user is setting an alarm time.
Referenced by main(), and refresh_display().
#define STRING_EOL "\r" |
#define STRING_HEADER |
Referenced by main().
|
static |
Configure the console UART.
References uart_rs232_options::baudrate, CONF_UART, CONF_UART_BAUDRATE, CONF_UART_CHAR_LENGTH, CONF_UART_PARITY, CONF_UART_STOP_BITS, CONSOLE_UART_ID, stdio_serial_init(), and sysclk_enable_peripheral_clock().
Referenced by main().
|
static |
RTT configuration function.
Configure the RTT to generate a one second tick, which triggers the RTTINC interrupt.
References rtt_enable_interrupt(), rtt_init(), rtt_read_timer_value(), and rtt_sel_source().
Referenced by main().
int main | ( | void | ) |
Application entry point for RTT example.
Initialize the RTT, display the current time and allow the user to perform several actions: clear the timer, set an alarm, etc.
References ASCII_BS, ASCII_CR, board_init(), configure_console(), configure_rtt(), g_uc_alarmed, g_uc_state, g_ul_new_alarm, refresh_display(), rtt_write_alarm_time(), STATE_MAIN_MENU, STATE_SET_ALARM, STRING_HEADER, and sysclk_init().
|
static |
Refresh display on terminal.
Update the terminal display to show the current menu and the current time depending on the device state.
References g_uc_alarmed, g_uc_state, g_ul_new_alarm, rtt_read_timer_value(), STATE_MAIN_MENU, and STATE_SET_ALARM.
Referenced by main(), and RTT_Handler().
void RTT_Handler | ( | void | ) |
Interrupt handler for the RTT.
Display the current time on the terminal.
References g_uc_alarmed, refresh_display(), and rtt_get_status().
volatile uint8_t g_uc_alarmed |
Indicate that an alarm has occurred but has not been cleared.
Referenced by main(), refresh_display(), and RTT_Handler().
volatile uint8_t g_uc_state |
Current device state.
Referenced by main(), and refresh_display().
volatile uint32_t g_ul_new_alarm |
New alarm time being currently entered.
Referenced by main(), and refresh_display().