Microchip® Advanced Software Framework

twi_eeprom_pdc_example.c File Reference

TWI EEPROM PDC Example for SAM.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

#include "asf.h"
#include "stdio_serial.h"
#include "conf_board.h"
#include "led.h"

Macros

#define AT24C_ADDRESS   0x40
 Address of AT24C chips. More...
 
#define EEPROM_MEM_ADDR   0
 
#define EEPROM_MEM_ADDR_LENGTH   2
 
#define STRING_EOL   "\r"
 
#define STRING_HEADER
 
#define TEST_DATA_LENGTH   (sizeof(test_data_tx)/sizeof(uint8_t))
 Data to be sent. More...
 
#define TWI_CLK   100000
 TWI Bus Clock 100kHz. More...
 
#define WAIT_TIME   10
 EEPROM Wait Time. More...
 

Functions

void BOARD_TWI_Handler (void)
 
static void configure_console (void)
 Configure the Console UART. More...
 
int main (void)
 Application entry point for TWI EEPROM example. More...
 
static void mdelay (uint32_t ul_dly_ticks)
 Wait for the given number of milliseconds (using the dwTimeStamp generated by the SAM microcontrollers' system tick). More...
 
void SysTick_Handler (void)
 Handler for System Tick interrupt. More...
 
static void twi_master_pdc_read (Twi *p_twi, twi_packet_t *p_packet)
 Read multiple bytes from a TWI compatible slave device. More...
 
static void twi_master_pdc_write (Twi *p_twi, twi_packet_t *p_packet)
 Write multiple bytes to a TWI compatible slave device. More...
 
static uint32_t twi_read_status (Twi *p_twi)
 Read status register. More...
 

Variables

Pdc * g_p_twim_pdc
 
volatile uint32_t g_ul_ms_ticks = 0
 Global timestamp in milliseconds since start of application. More...
 
static uint8_t gs_uc_test_data_rx [TEST_DATA_LENGTH] = { 0 }
 Reception buffer. More...
 
twi_packet_t packet_rx
 
twi_packet_t packet_tx
 Define TX and RX packet. More...
 
volatile uint32_t Read_Interrupt_Flag = 0
 
static const volatile uint8_t test_data_tx []
 
volatile uint32_t Write_Interrupt_Flag = 0
 Define interrupt flag. More...
 

#define AT24C_ADDRESS   0x40

Address of AT24C chips.

Referenced by main().

#define EEPROM_MEM_ADDR   0

Referenced by main().

#define EEPROM_MEM_ADDR_LENGTH   2

Referenced by main().

#define STRING_EOL   "\r"
#define STRING_HEADER
Value:
"--TWI EEPROM Example --\r\n" \
"-- "BOARD_NAME" --\r\n" \
"-- Compiled: "__DATE__" "__TIME__" --"STRING_EOL
#define STRING_EOL
Definition: twi_eeprom_pdc_example.c:110
#define BOARD_NAME
Definition: sam3x_ek.h:81

Referenced by main().

#define TEST_DATA_LENGTH   (sizeof(test_data_tx)/sizeof(uint8_t))

Data to be sent.

Referenced by main().

#define TWI_CLK   100000

TWI Bus Clock 100kHz.

Referenced by main().

#define WAIT_TIME   10

EEPROM Wait Time.

Referenced by main().

void BOARD_TWI_Handler ( void  )
static void configure_console ( void  )
static
static void mdelay ( uint32_t  ul_dly_ticks)
static

Wait for the given number of milliseconds (using the dwTimeStamp generated by the SAM microcontrollers' system tick).

Parameters
ul_dly_ticksDelay to wait for, in milliseconds.

References g_ul_ms_ticks.

Referenced by main().

void SysTick_Handler ( void  )

Handler for System Tick interrupt.

Process System Tick Event increments the timestamp counter.

static void twi_master_pdc_read ( Twi *  p_twi,
twi_packet_t p_packet 
)
static

Read multiple bytes from a TWI compatible slave device.

Parameters
p_twiPointer to a TWI instance.
p_packetPacket information and data (see twi_packet_t).

References twi_packet::addr, twi_packet::addr_length, BOARD_BASE_TWI_EEPROM, twi_packet::buffer, twi_packet::chip, twi_packet::length, pdc_disable_transfer(), pdc_enable_transfer(), pdc_rx_init(), twi_enable_interrupt(), twi_mk_addr(), twi_read_status(), pdc_packet::ul_addr, and pdc_packet::ul_size.

Referenced by main().

static void twi_master_pdc_write ( Twi *  p_twi,
twi_packet_t p_packet 
)
static

Write multiple bytes to a TWI compatible slave device.

Parameters
p_twiPointer to a TWI instance.
p_packetPacket information and data (see twi_packet_t).

References twi_packet::addr, twi_packet::addr_length, BOARD_BASE_TWI_EEPROM, twi_packet::buffer, twi_packet::chip, twi_packet::length, pdc_disable_transfer(), pdc_enable_transfer(), pdc_tx_init(), twi_enable_interrupt(), twi_mk_addr(), twi_read_status(), pdc_packet::ul_addr, and pdc_packet::ul_size.

Referenced by main().

static uint32_t twi_read_status ( Twi *  p_twi)
inlinestatic

Read status register.

Parameters
p_twiPointer to an TWI instance.
Returns
TWI status register value.

Referenced by twi_master_pdc_read(), and twi_master_pdc_write().

Pdc* g_p_twim_pdc
volatile uint32_t g_ul_ms_ticks = 0

Global timestamp in milliseconds since start of application.

Referenced by mdelay().

uint8_t gs_uc_test_data_rx[TEST_DATA_LENGTH] = { 0 }
static

Reception buffer.

Referenced by main().

twi_packet_t packet_rx
twi_packet_t packet_tx

Define TX and RX packet.

volatile uint32_t Read_Interrupt_Flag = 0
const volatile uint8_t test_data_tx[]
static
Initial value:
= {
'S', 'A', 'M', ' ', 'T', 'W', 'I', ' ',
'E', 'E', 'P', 'R', 'O', 'M', ' ',
'E', 'X', 'A', 'M', 'P', 'L', 'E'
}
volatile uint32_t Write_Interrupt_Flag = 0

Define interrupt flag.