Two-Wire Interface (TWI) driver for SAM.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
Data Structures | |
struct | twi_options |
Input parameters when initializing the TWI module mode. More... | |
struct | twi_packet |
Information concerning the data transmission. More... | |
Macros | |
#define | TWI_TIMEOUT 30000 |
Time-out value (number of attempts). More... | |
#define | TWI_SUCCESS 0 |
Return codes for TWI APIs. More... | |
#define | TWI_INVALID_ARGUMENT 1 |
#define | TWI_ARBITRATION_LOST 2 |
#define | TWI_NO_CHIP_FOUND 3 |
#define | TWI_RECEIVE_OVERRUN 4 |
#define | TWI_RECEIVE_NACK 5 |
#define | TWI_SEND_OVERRUN 6 |
#define | TWI_SEND_NACK 7 |
#define | TWI_BUSY 8 |
#define | TWI_ERROR_TIMEOUT 9 |
Typedefs | |
typedef struct twi_options | twi_options_t |
Input parameters when initializing the TWI module mode. More... | |
typedef struct twi_packet | twi_packet_t |
Information concerning the data transmission. More... | |
Enumerations | |
enum | twi_source_clock { TWI_SOURCE_PERIPH_CLK = TWI_CWGR_BRSRCCLK_PERIPH_CLK, TWI_SOURCE_PCK_CLK = TWI_CWGR_BRSRCCLK_PMC_PCK } |
Functions | |
static void | twi_clear_disable_clock_wait_state (Twi *p_twi) |
Clear clock wait state disable mode. More... | |
static void | twi_disable_alternative_command (Twi *p_twi) |
Enable alternative command mode. More... | |
static void | twi_disable_clock_wait_state (Twi *p_twi) |
Clock stretching disabled in slave mode, OVRE and UNRE will indicate overrun and underrun. More... | |
static void | twi_disable_highspeed (Twi *p_twi) |
Disable high speed mode. More... | |
void | twi_disable_interrupt (Twi *p_twi, uint32_t ul_sources) |
Disable TWI interrupts. More... | |
void | twi_disable_master_mode (Twi *p_twi) |
Disable TWI master mode. More... | |
static void | twi_disable_pec (Twi *p_twi) |
Disable packet error checking. More... | |
static void | twi_disable_slave_addr1_matching (Twi *p_twi) |
Slave Address 1 matching disabled. More... | |
static void | twi_disable_slave_addr2_matching (Twi *p_twi) |
Slave Address 2 matching disabled. More... | |
static void | twi_disable_slave_addr3_matching (Twi *p_twi) |
Slave Address 3 matching disabled. More... | |
static void | twi_disable_slave_data_matching (Twi *p_twi) |
First received data matching disabled. More... | |
static void | twi_disable_slave_default_addr (Twi *p_twi) |
Acknowledge of the SMBus Default Address disabled. More... | |
void | twi_disable_slave_mode (Twi *p_twi) |
Disable TWI slave mode. More... | |
static void | twi_disable_slave_nack (Twi *p_twi) |
Normal value to be returned in the ACK cycle of the data phase in slave receiver mode. More... | |
static void | twi_disable_smbus (Twi *p_twi) |
Disable SMBus mode. More... | |
static void | twi_disable_smbus_host_header (Twi *p_twi) |
Acknowledge of the SMBus Host Header disabled. More... | |
static void | twi_enable_alternative_command (Twi *p_twi) |
Enable alternative command mode. More... | |
static void | twi_enable_highspeed (Twi *p_twi) |
Enable high speed mode. More... | |
void | twi_enable_interrupt (Twi *p_twi, uint32_t ul_sources) |
Enable TWI interrupts. More... | |
void | twi_enable_master_mode (Twi *p_twi) |
Enable TWI master mode. More... | |
static void | twi_enable_pec (Twi *p_twi) |
Enable packet error checking. More... | |
static void | twi_enable_slave_addr1_matching (Twi *p_twi) |
Slave Address 1 matching enabled. More... | |
static void | twi_enable_slave_addr2_matching (Twi *p_twi) |
Slave Address 2 matching enabled. More... | |
static void | twi_enable_slave_addr3_matching (Twi *p_twi) |
Slave Address 3 matching enabled. More... | |
static void | twi_enable_slave_default_addr (Twi *p_twi) |
Acknowledge of the SMBus Default Address enabled. More... | |
void | twi_enable_slave_mode (Twi *p_twi) |
Enable TWI slave mode. More... | |
static void | twi_enable_slave_nack (Twi *p_twi) |
NACK value to be returned in the ACK cycle of the data phase in slave receiver mode. More... | |
static void | twi_enable_smbus (Twi *p_twi) |
Enable SMBus mode. More... | |
static void | twi_enable_smbus_host_header (Twi *p_twi) |
Acknowledge of the SMBus Host Header enabled. More... | |
uint32_t | twi_get_interrupt_mask (Twi *p_twi) |
Read TWI interrupt mask. More... | |
uint32_t | twi_get_interrupt_status (Twi *p_twi) |
Get TWI interrupt status. More... | |
Pdc * | twi_get_pdc_base (Twi *p_twi) |
Get TWI PDC base address. More... | |
static void | twi_lock_clear (Twi *p_twi) |
Clear the TWI FSM lock. More... | |
void | twi_mask_slave_addr (Twi *p_twi, uint32_t ul_mask) |
uint32_t | twi_master_init (Twi *p_twi, const twi_options_t *p_opt) |
Initialize TWI master mode. More... | |
uint32_t | twi_master_read (Twi *p_twi, twi_packet_t *p_packet) |
Read multiple bytes from a TWI compatible slave device. More... | |
uint32_t | twi_master_write (Twi *p_twi, twi_packet_t *p_packet) |
Write multiple bytes to a TWI compatible slave device. More... | |
uint32_t | twi_mk_addr (const uint8_t *addr, int len) |
Construct the TWI module address register field. More... | |
uint32_t | twi_probe (Twi *p_twi, uint8_t uc_slave_addr) |
Test if a chip answers a given I2C address. More... | |
uint8_t | twi_read_byte (Twi *p_twi) |
Reads a byte from the TWI bus. More... | |
void | twi_read_write_protection_status (Twi *p_twi, uint32_t *p_status) |
static void | twi_request_pec (Twi *p_twi) |
Request a packet error checking. More... | |
void | twi_reset (Twi *p_twi) |
Reset TWI. More... | |
static void | twi_select_source_clock (Twi *p_twi, enum twi_source_clock src_clk) |
Select the souce clock for the bit rate generation. More... | |
static void | twi_send_clear (Twi *p_twi) |
If master mode is enabled, send a bus clear command. More... | |
void | twi_set_alternative_command (Twi *p_twi, uint32_t ul_alt_cmd) |
void | twi_set_filter (Twi *p_twi, uint32_t ul_filter) |
void | twi_set_slave_addr (Twi *p_twi, uint32_t ul_device_addr) |
Set TWI slave address. More... | |
void | twi_set_sleepwalking (Twi *p_twi, uint32_t ul_matching_addr1, bool flag1, uint32_t ul_matching_addr2, bool flag2, uint32_t ul_matching_addr3, bool flag3, uint32_t ul_matching_data, bool flag) |
uint32_t | twi_set_speed (Twi *p_twi, uint32_t ul_speed, uint32_t ul_mck) |
Set the I2C bus speed in conjunction with the clock frequency. More... | |
void | twi_set_write_protection (Twi *p_twi, bool flag) |
void | twi_slave_init (Twi *p_twi, uint32_t ul_device_addr) |
Initialize TWI slave mode. More... | |
uint32_t | twi_slave_read (Twi *p_twi, uint8_t *p_data) |
Read data from master. More... | |
uint32_t | twi_slave_write (Twi *p_twi, uint8_t *p_data) |
Write data to TWI bus. More... | |
void | twi_smbus_set_timing (Twi *p_twi, uint32_t ul_timing) |
static void | twi_thr_clear (Twi *p_twi) |
Clear the Transmit Holding Register and set TXRDY, TXCOMP flags. More... | |
void | twi_write_byte (Twi *p_twi, uint8_t uc_byte) |
Sends a byte of data to one of the TWI slaves on the bus. More... | |
#define TWI_ARBITRATION_LOST 2 |
#define TWI_BUSY 8 |
#define TWI_ERROR_TIMEOUT 9 |
Referenced by twi_master_read().
#define TWI_INVALID_ARGUMENT 1 |
Referenced by twi_master_init(), twi_master_read(), and twi_master_write().
#define TWI_NO_CHIP_FOUND 3 |
#define TWI_RECEIVE_NACK 5 |
Referenced by twi_master_read(), and twi_master_write().
#define TWI_RECEIVE_OVERRUN 4 |
#define TWI_SEND_NACK 7 |
#define TWI_SEND_OVERRUN 6 |
#define TWI_SUCCESS 0 |
Return codes for TWI APIs.
Referenced by twi_master_init(), twi_master_read(), and twi_master_write().
#define TWI_TIMEOUT 30000 |
Time-out value (number of attempts).
Referenced by twi_master_read().
typedef struct twi_options twi_options_t |
Input parameters when initializing the TWI module mode.
typedef struct twi_packet twi_packet_t |
Information concerning the data transmission.
enum twi_source_clock |
|
inlinestatic |
Clear clock wait state disable mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Enable alternative command mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Clock stretching disabled in slave mode, OVRE and UNRE will indicate overrun and underrun.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Disable high speed mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Disable packet error checking.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Slave Address 1 matching disabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Slave Address 2 matching disabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Slave Address 3 matching disabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
First received data matching disabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Acknowledge of the SMBus Default Address disabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Normal value to be returned in the ACK cycle of the data phase in slave receiver mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Disable SMBus mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Acknowledge of the SMBus Host Header disabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Enable alternative command mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Enable high speed mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Enable packet error checking.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Slave Address 1 matching enabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Slave Address 2 matching enabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Slave Address 3 matching enabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Acknowledge of the SMBus Default Address enabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
NACK value to be returned in the ACK cycle of the data phase in slave receiver mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Enable SMBus mode.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Acknowledge of the SMBus Host Header enabled.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Clear the TWI FSM lock.
p_twi | Base address of the TWI instance. |
void twi_mask_slave_addr | ( | Twi * | p_twi, |
uint32_t | ul_mask | ||
) |
void twi_read_write_protection_status | ( | Twi * | p_twi, |
uint32_t * | p_status | ||
) |
|
inlinestatic |
Request a packet error checking.
p_twi | Base address of the TWI instance. |
|
inlinestatic |
Select the souce clock for the bit rate generation.
p_twi | Base address of the TWI instance. |
src_clk | Source clock. |
|
inlinestatic |
If master mode is enabled, send a bus clear command.
p_twi | Base address of the TWI instance. |
void twi_set_alternative_command | ( | Twi * | p_twi, |
uint32_t | ul_alt_cmd | ||
) |
void twi_set_filter | ( | Twi * | p_twi, |
uint32_t | ul_filter | ||
) |
void twi_set_sleepwalking | ( | Twi * | p_twi, |
uint32_t | ul_matching_addr1, | ||
bool | flag1, | ||
uint32_t | ul_matching_addr2, | ||
bool | flag2, | ||
uint32_t | ul_matching_addr3, | ||
bool | flag3, | ||
uint32_t | ul_matching_data, | ||
bool | flag | ||
) |
void twi_set_write_protection | ( | Twi * | p_twi, |
bool | flag | ||
) |
void twi_smbus_set_timing | ( | Twi * | p_twi, |
uint32_t | ul_timing | ||
) |
|
inlinestatic |
Clear the Transmit Holding Register and set TXRDY, TXCOMP flags.
p_twi | Base address of the TWI instance. |