Microchip® Advanced Software Framework

usart_rs485_example_canopus.c File Reference

USART RS485 example for SAM.

Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.

#include <string.h>
#include "asf.h"
#include "stdio_serial.h"
#include "conf_board.h"
#include "conf_clock.h"
#include "conf_example.h"

Macros

#define ACK_CHAR   0x13
 Character to acknowledge receipt of the sync char. More...
 
#define ALL_INTERRUPT_MASK   0xffffffff
 All interrupt mask. More...
 
#define BUFFER_SIZE   2000
 Size of the receive buffer and transmit buffer. More...
 
#define PDC_BUF_SIZE   BUFFER_SIZE
 Size of the buffer. More...
 
#define STRING_EOL   "\r"
 
#define STRING_HEADER
 
#define SYNC_CHAR   0x11
 Character to synchronize with the other end. More...
 
#define SYS_TICK_FREQ   1000
 System tick frequency in Hz. More...
 
#define TIMEOUT   (1000)
 Acknowledge time out. More...
 

Typedefs

typedef enum st_usart_state usart_state_t
 State of the USART. More...
 

Enumerations

enum  st_usart_state {
  INITIALIZED,
  TRANSMITTING,
  RECEIVING,
  RECEIVED,
  TRANSMITTED
}
 State of the USART. More...
 

Functions

static void configure_console (void)
 Configure UART for debug message output. More...
 
static void configure_systick (void)
 Configure system tick to generate an interrupt every 1ms. More...
 
static void configure_usart (void)
 USART RS485 mode configuration. More...
 
static void dump_info (char *p_buf, uint32_t ul_size)
 Dump buffer to uart. More...
 
static uint8_t func_transmit (const uint8_t *p_buff, uint32_t ulsize)
 transmit data. More...
 
static uint32_t get_tick_count (void)
 Get the tick count value. More...
 
int main (void)
 usart_rs485 Application entry point. More...
 
void SysTick_Handler (void)
 Handler for System Tick interrupt. More...
 
void USART_Handler (void)
 Handler for USART interrupt. More...
 
static void wait (volatile uint32_t ul_ms)
 Wait for some time in ms. More...
 

Variables

volatile usart_state_t g_state = INITIALIZED
 Global usart state. More...
 
uint8_t g_uc_receive_buffer [BUFFER_SIZE]
 Receive buffer. More...
 
uint8_t g_uc_transmit_buffer [BUFFER_SIZE]
 Transmit buffer. More...
 
volatile uint32_t g_ul_tick_count
 Tick Counter in unit of ms. More...
 
uint32_t g_ulcount = 0
 count number for received data. More...
 
uint8_t * p_revdata = &g_uc_receive_buffer[0]
 Pointer to receive buffer base. More...
 

#define ACK_CHAR   0x13

Character to acknowledge receipt of the sync char.

Referenced by main().

#define ALL_INTERRUPT_MASK   0xffffffff

All interrupt mask.

Referenced by configure_usart().

#define BUFFER_SIZE   2000

Size of the receive buffer and transmit buffer.

Referenced by main(), and USART_Handler().

#define PDC_BUF_SIZE   BUFFER_SIZE

Size of the buffer.

#define STRING_EOL   "\r"
#define STRING_HEADER
Value:
"-- USART RS485 Example --\r\n" \
"-- "BOARD_NAME" --\r\n" \
"-- Compiled: "__DATE__" "__TIME__" --"STRING_EOL
#define BOARD_NAME
Name of the board.
Definition: samv71_xplained_ultra.h:75
#define STRING_EOL
Definition: usart_rs485_example_canopus.c:146

Referenced by main().

#define SYNC_CHAR   0x11

Character to synchronize with the other end.

Referenced by main().

#define SYS_TICK_FREQ   1000

System tick frequency in Hz.

Referenced by configure_systick().

#define TIMEOUT   (1000)

Acknowledge time out.

Referenced by main().

State of the USART.

State of the USART.

Enumerator
INITIALIZED 
TRANSMITTING 
RECEIVING 
RECEIVED 
TRANSMITTED 

static void configure_console ( void  )
static
static void configure_systick ( void  )
static

Configure system tick to generate an interrupt every 1ms.

References SYS_TICK_FREQ, and sysclk_get_cpu_hz().

Referenced by main().

static void configure_usart ( void  )
static

USART RS485 mode configuration.

Configure USART in RS485 mode, asynchronous, 8 bits, 1 stop bit, no parity, 256000 bauds and enable its transmitter and receiver.

References ALL_INTERRUPT_MASK, BOARD_ID_USART, BOARD_USART, BOARD_USART_BAUDRATE, sysclk_enable_peripheral_clock(), sysclk_get_peripheral_hz(), usart_disable_interrupt(), usart_enable_rx(), usart_enable_tx(), usart_init_rs485(), USART_IRQn, and usart_set_tx_timeguard().

Referenced by main().

static void dump_info ( char *  p_buf,
uint32_t  ul_size 
)
static

Dump buffer to uart.

Referenced by main().

static uint8_t func_transmit ( const uint8_t *  p_buff,
uint32_t  ulsize 
)
static

transmit data.

Parameters
*p_buffdata to be transmitted
ulsizesize of all data.

References Assert, BOARD_USART, usart_enable_interrupt(), usart_is_tx_empty(), and usart_write().

Referenced by main().

static uint32_t get_tick_count ( void  )
static

Get the tick count value.

References g_ul_tick_count.

Referenced by main().

int main ( void  )

usart_rs485 Application entry point.

Configure USART in RS485 mode. If the application starts earlier, it acts as a receiver. Otherwise, it should be a transmitter.

Returns
Unused (ANSI-C compatibility).

References ACK_CHAR, board_init(), BOARD_USART, BUFFER_SIZE, configure_console(), configure_systick(), configure_usart(), dump_info(), func_transmit(), g_state, g_uc_receive_buffer, g_uc_transmit_buffer, get_tick_count(), RECEIVED, RECEIVING, STRING_HEADER, SYNC_CHAR, sysclk_init(), TIMEOUT, TRANSMITTING, usart_disable_rx(), usart_enable_interrupt(), usart_enable_rx(), usart_enable_tx(), usart_is_rx_ready(), usart_read(), and wait().

void SysTick_Handler ( void  )

Handler for System Tick interrupt.

Process System Tick Event. Increment the ul_ms_ticks counter.

References g_ul_tick_count.

void USART_Handler ( void  )
static void wait ( volatile uint32_t  ul_ms)
static

Wait for some time in ms.

References g_ul_tick_count.

Referenced by main().

volatile usart_state_t g_state = INITIALIZED

Global usart state.

Referenced by main(), and USART_Handler().

uint8_t g_uc_receive_buffer[BUFFER_SIZE]

Receive buffer.

Referenced by main().

uint8_t g_uc_transmit_buffer[BUFFER_SIZE]
Initial value:
= "DESCRIPTION of this example: \r\n \
**************************************************************************\r\n\
* This application gives an example of how to use USART in RS485 mode.\r\n\
* RS-485 is a standard defining the electrical characteristics of drivers \r\n\
* and receivers for use in balanced digital multipoint systems. The standard \r\n\
* is published by the ANSI TIA/EIA. \r\n\
* \r\n\
* This example connects two boards through RS485 interface. One board acts \r\n\
* as the transmitter and the other one as the receiver. It is determined by \r\n\
* the sequence the two applications started. The earlier started board will \r\n\
* act automatically as the receiver due to no acknowledgement received. The \r\n\
* receiver will wait until sync character is received. Then it sends the \r\n\
* acknowledgement and waits for the full frame sent by the transmitter. \r\n\
* At the end of reception, it prints out message through UART interface to \r\n\
* assert that the whole process succeeds.\r\n\
**************************************************************************\r\n\
END of DESCRIPTION \r\n\
"

Transmit buffer.

Pure ASCII text.

Referenced by main().

volatile uint32_t g_ul_tick_count

Tick Counter in unit of ms.

Referenced by get_tick_count(), SysTick_Handler(), and wait().

uint32_t g_ulcount = 0

count number for received data.

Referenced by USART_Handler().

uint8_t* p_revdata = &g_uc_receive_buffer[0]

Pointer to receive buffer base.

Referenced by USART_Handler().