Symbols to use for configuring the board and its initialization.
Initialization | |
#define | CONF_BOARD_KEEP_WATCHDOG_AT_INIT |
Define to avoid disabling the watchdog at startup. More... | |
#define CONF_BOARD_KEEP_WATCHDOG_AT_INIT |
Define to avoid disabling the watchdog at startup.
Let watchdog remain enabled.
If this symbol is defined, the watchdog is left running with its current configuration. Otherwise, it gets disabled during board initialization.