SPI master common service for SAM.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
#include "sysclk.h"
#include "status_codes.h"
#include "spi.h"
#include "conf_spi_master.h"
Data Structures | |
struct | spi_device |
Polled SPI device definition. More... | |
Macros | |
#define | SPI_CPHA (1 << 0) |
Default Configuration of SPI Master Delay BCS. More... | |
#define | SPI_CPOL (1 << 1) |
Clock polarity. More... | |
#define | SPI_MODE_0 0 |
SPI mode 0. More... | |
#define | SPI_MODE_1 (SPI_CPHA) |
SPI mode 1. More... | |
#define | SPI_MODE_2 (SPI_CPOL) |
SPI mode 2. More... | |
#define | SPI_MODE_3 (SPI_CPOL | SPI_CPHA) |
SPI mode 3. More... | |
#define | SPI_TYPE_DEFS |
Typedefs | |
typedef uint32_t | board_spi_select_id_t |
Board SPI Select Id Definition. More... | |
typedef uint8_t | spi_flags_t |
SPI Flags Definition. More... | |
Functions | |
void | spi_deselect_device (Spi *p_spi, struct spi_device *device) |
Deselect the given device on the SPI bus. More... | |
void | spi_master_init (Spi *p_spi) |
Initialize the SPI in master mode. More... | |
void | spi_master_setup_device (Spi *p_spi, struct spi_device *device, spi_flags_t flags, uint32_t baud_rate, board_spi_select_id_t sel_id) |
Set up an SPI device. More... | |
status_code_t | spi_read_packet (Spi *p_spi, uint8_t *data, size_t len) |
Receive a sequence of bytes from an SPI device. More... | |
static void | spi_read_single (Spi *p_spi, uint8_t *data) |
Receive one byte from an SPI device. More... | |
void | spi_select_device (Spi *p_spi, struct spi_device *device) |
Select the given device on the SPI bus. More... | |
status_code_t | spi_transceive_packet (Spi *p_spi, uint8_t *tx_data, uint8_t *rx_data, size_t len) |
Send and receive a sequence of bytes from an SPI device. More... | |
status_code_t | spi_write_packet (Spi *p_spi, const uint8_t *data, size_t len) |
Send a sequence of bytes to an SPI device. More... | |
static void | spi_write_single (Spi *p_spi, uint8_t data) |
Write one byte to an SPI device. More... | |
#define SPI_CPHA (1 << 0) |
Default Configuration of SPI Master Delay BCS.
Default Configuration of SPI Master Bits per Transfer Definition Default Configuration of SPI Master Delay BCT Default Configuration of SPI Master Delay BS Default Configuration of SPI Master Dummy Field Clock phase.
#define SPI_CPOL (1 << 1) |
Clock polarity.
#define SPI_MODE_0 0 |
SPI mode 0.
Referenced by ads7843_init(), usart_init_spi_master(), and usart_init_spi_slave().
#define SPI_MODE_1 (SPI_CPHA) |
SPI mode 1.
Referenced by usart_init_spi_master(), and usart_init_spi_slave().
#define SPI_MODE_2 (SPI_CPOL) |
SPI mode 2.
Referenced by usart_init_spi_master(), and usart_init_spi_slave().
SPI mode 3.
Referenced by usart_init_spi_master(), and usart_init_spi_slave().
#define SPI_TYPE_DEFS |
typedef uint32_t board_spi_select_id_t |
Board SPI Select Id Definition.
typedef uint8_t spi_flags_t |
SPI Flags Definition.
void spi_deselect_device | ( | Spi * | p_spi, |
struct spi_device * | device | ||
) |
Deselect the given device on the SPI bus.
Call board chip deselect.
p_spi | Base address of the SPI instance. |
device | SPI device. |
References NONE_CHIP_SELECT_ID, spi_is_tx_empty(), spi_set_lastxfer(), spi_set_peripheral_chip_select_value(), and UNUSED.
void spi_master_init | ( | Spi * | p_spi | ) |
Initialize the SPI in master mode.
p_spi | Base address of the SPI instance. |
References CONFIG_SPI_MASTER_DELAY_BCS, DEFAULT_CHIP_ID, spi_disable_loopback(), spi_disable_mode_fault_detect(), spi_disable_peripheral_select_decode(), spi_enable_clock(), spi_reset(), spi_set_delay_between_chip_select(), spi_set_fixed_peripheral_select(), spi_set_master_mode(), and spi_set_peripheral_chip_select_value().
Referenced by ads7843_init().
void spi_master_setup_device | ( | Spi * | p_spi, |
struct spi_device * | device, | ||
spi_flags_t | flags, | ||
uint32_t | baud_rate, | ||
board_spi_select_id_t | sel_id | ||
) |
Set up an SPI device.
The returned device descriptor structure must be passed to the driver whenever that device should be used as current slave device.
p_spi | Base address of the SPI instance. |
device | Pointer to SPI device struct that should be initialized. |
flags | SPI configuration flags. Common flags for all implementations are the SPI modes SPI_MODE_0 ... SPI_MODE_3. |
baud_rate | Baud rate for communication with slave device in Hz. |
sel_id | Board specific select id. |
References Assert, CONFIG_SPI_MASTER_BITS_PER_TRANSFER, CONFIG_SPI_MASTER_DELAY_BCT, CONFIG_SPI_MASTER_DELAY_BS, spi_device::id, spi_calc_baudrate_div(), spi_configure_cs_behavior(), SPI_CS_KEEP_LOW, spi_set_baudrate_div(), spi_set_bits_per_transfer(), spi_set_clock_phase(), spi_set_clock_polarity(), spi_set_transfer_delay(), sysclk_get_peripheral_hz(), and UNUSED.
Referenced by ads7843_init().
status_code_t spi_read_packet | ( | Spi * | p_spi, |
uint8_t * | data, | ||
size_t | len | ||
) |
Receive a sequence of bytes from an SPI device.
All bytes sent out on SPI bus are sent as value 0xff.
p_spi | Base address of the SPI instance. |
data | Data buffer to read. |
len | Length of data to be read. |
All bytes sent out on SPI bus are sent as value 0.
p_spi | Base address of the SPI instance. |
data | Data buffer to read. |
len | Length of data to be read. |
References CONFIG_SPI_MASTER_DUMMY, ERR_TIMEOUT, spi_is_rx_ready(), spi_is_tx_ready(), spi_read_single(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.
|
inlinestatic |
Receive one byte from an SPI device.
p_spi | Base address of the SPI instance. |
data | Data to read. |
References spi_get().
Referenced by ads7843_send_cmd(), spi_read_packet(), and spi_transceive_packet().
void spi_select_device | ( | Spi * | p_spi, |
struct spi_device * | device | ||
) |
Select the given device on the SPI bus.
Set device specific setting and call board chip select.
p_spi | Base address of the SPI instance. |
device | SPI device. |
References spi_device::id, MAX_NUM_WITH_DECODER, MAX_NUM_WITHOUT_DECODER, spi_get_peripheral_select_decode_setting(), and spi_set_peripheral_chip_select_value().
Referenced by ads7843_init().
status_code_t spi_transceive_packet | ( | Spi * | p_spi, |
uint8_t * | tx_data, | ||
uint8_t * | rx_data, | ||
size_t | len | ||
) |
Send and receive a sequence of bytes from an SPI device.
p_spi | Base address of the SPI instance. |
tx_data | Data buffer to send. |
rx_data | Data buffer to read. |
len | Length of data to be read. |
References ERR_TIMEOUT, spi_is_rx_ready(), spi_is_tx_ready(), spi_read_single(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.
status_code_t spi_write_packet | ( | Spi * | p_spi, |
const uint8_t * | data, | ||
size_t | len | ||
) |
Send a sequence of bytes to an SPI device.
Received bytes on the SPI bus are discarded.
p_spi | Base address of the SPI instance. |
data | Data buffer to write. |
len | Length of data to be written. |
References ERR_TIMEOUT, spi_is_tx_ready(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.
|
inlinestatic |
Write one byte to an SPI device.
p_spi | Base address of the SPI instance. |
data | Data to write. |
References spi_put().
Referenced by ads7843_send_cmd(), spi_read_packet(), spi_transceive_packet(), and spi_write_packet().