The cm4-bitbanding example will help new users get familiar with bitbanding feature of SAM4 microcontrollers.
Bit-banding is a useful feature of Cortex M4 processor. The processor memory map includes two bit-band regions, which occupy the lowest 1MB of the SRAM and Peripheral memory regions. These bit-band regions map each word in an alias region of memory to a bit in a bit-band region of memory.
The example will execute the following tests:
This package can be used with SAM4 evaluation kits.
The cm4-bitbanding example will help new users get familiar with bitbanding feature of SAM4 microcontrollers.