Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
CMSIS Example

Purpose

The cmsis example will help new users get familiar with basic cmsis utilities of SAM4 microcontrollers.

The example will execute the following tests:

  • The application will flash the LED per second. The second is calculated by the standard system tick interface of cmsis.

Requirements

This package can be used with SAM4 evaluation kits.

Description

The cmsis example will use the system tick of the Cortex-M4.

Usage

  1. Build the program and download it into the evaluation board.