Board configuration.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "system_sam4s.h"
Macros | |
#define | CONF_BOARD_UART_CONSOLE |
Configure UART on board. More... | |
#define | CONSOLE_UART_ID ID_UART0 |
Usart Hw ID used by the console (UART0). More... | |
#define | LED0_MASK (uint32_t)(0x01 << 19) |
#define | LED0_PIO PIOA |
#define | LED1_MASK (uint32_t)(0x01 << 20) |
#define | LED1_PIO PIOA |
#define CONF_BOARD_UART_CONSOLE |
Configure UART on board.
#define CONSOLE_UART_ID ID_UART0 |
Usart Hw ID used by the console (UART0).
Referenced by configure_console().
#define LED0_MASK (uint32_t)(0x01 << 19) |
#define LED0_PIO PIOA |
#define LED1_MASK (uint32_t)(0x01 << 20) |
#define LED1_PIO PIOA |