Microchip® Advanced Software Framework

Extra Information

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
EEPROM Electronically Erasable Read-Only Memory
NVM Non-Volatile Memory

Dependencies

This driver has the following dependencies:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Fix warnings
Initial Release