Below is a table listing the acronym used in this module, along with their intended meaning.
Acronym | Description |
---|---|
TSENS | Temperature Sensor |
This driver has no dependencies.
Errata reference: 14476.
The magnitude of the temperature measurement value decreases with increasing temperature, i.e. it has a negative temperature coefficient.
An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.
Changelog |
---|
Initial Release |