CCL LUT 0 to 3 configuration structure.
Configuration structure for CCL LUT 0 to 3.
#include <ccl.h>
Data Fields | |
bool | edge_selection_enable |
If true , Edge detector is enabled. More... | |
bool | event_input_enable |
If true , LUT incoming event is enabled. More... | |
bool | event_input_inverted_enable |
If true , incoming event is inverted. More... | |
bool | event_output_enable |
If true , LUT event output is enabled. More... | |
enum ccl_lut_filter_sel | filter_sel |
Selection of the LUT output filter options. More... | |
enum ccl_lut_input_src_sel | input0_src_sel |
Selection of the input0 source. More... | |
enum ccl_lut_input_src_sel | input1_src_sel |
Selection of the input1 source. More... | |
enum ccl_lut_input_src_sel | input2_src_sel |
Selection of the input2 source. More... | |
uint8_t | truth_table_value |
The value of truth logic as a function of inputs IN[2:0]. More... | |
bool ccl_lut_config::edge_selection_enable |
If true
, Edge detector is enabled.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
bool ccl_lut_config::event_input_enable |
If true
, LUT incoming event is enabled.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
bool ccl_lut_config::event_input_inverted_enable |
If true
, incoming event is inverted.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
bool ccl_lut_config::event_output_enable |
If true
, LUT event output is enabled.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
enum ccl_lut_filter_sel ccl_lut_config::filter_sel |
Selection of the LUT output filter options.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
enum ccl_lut_input_src_sel ccl_lut_config::input0_src_sel |
Selection of the input0 source.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
enum ccl_lut_input_src_sel ccl_lut_config::input1_src_sel |
Selection of the input1 source.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
enum ccl_lut_input_src_sel ccl_lut_config::input2_src_sel |
Selection of the input2 source.
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().
uint8_t ccl_lut_config::truth_table_value |
The value of truth logic as a function of inputs IN[2:0].
Referenced by ccl_lut_get_config_defaults(), and ccl_lut_set_config().