Configuration struct for TCC module recoverable fault.
#include <tcc.h>
Data Fields | |
enum tcc_fault_blanking | blanking |
Fault Blanking Start Point for recoverable Fault. More... | |
uint8_t | blanking_cycles |
Fault blanking value (0 ~ 255), disable input source for several TCC clocks after the detection of the waveform edge. More... | |
enum tcc_fault_capture_action | capture_action |
Capture action for recoverable Fault. More... | |
enum tcc_fault_capture_channel | capture_channel |
Channel triggered by recoverable Fault. More... | |
uint8_t | filter_value |
Fault filter value applied on MCEx event input line (0x0 ~ 0xF). More... | |
enum tcc_fault_halt_action | halt_action |
Halt action for recoverable Fault. More... | |
bool | keep |
Set to true to enable keep action (keep until end of TCC cycle) More... | |
bool | qualification |
Set to true to enable input qualification (disable input when output is inactive) More... | |
bool | restart |
Set to true to enable restart action. More... | |
enum tcc_fault_source | source |
Specifies if the event input generates recoverable Fault. More... | |
enum tcc_fault_blanking tcc_recoverable_fault_config::blanking |
Fault Blanking Start Point for recoverable Fault.
Referenced by _tcc_build_faults().
uint8_t tcc_recoverable_fault_config::blanking_cycles |
Fault blanking value (0 ~ 255), disable input source for several TCC clocks after the detection of the waveform edge.
Referenced by _tcc_build_faults().
enum tcc_fault_capture_action tcc_recoverable_fault_config::capture_action |
Capture action for recoverable Fault.
Referenced by _tcc_build_faults().
enum tcc_fault_capture_channel tcc_recoverable_fault_config::capture_channel |
Channel triggered by recoverable Fault.
Referenced by _tcc_build_faults().
uint8_t tcc_recoverable_fault_config::filter_value |
Fault filter value applied on MCEx event input line (0x0 ~ 0xF).
Must be 0 when MCEx event is used as synchronous event. Apply to both recoverable and non-recoverable fault.
Referenced by _tcc_build_faults().
enum tcc_fault_halt_action tcc_recoverable_fault_config::halt_action |
Halt action for recoverable Fault.
Referenced by _tcc_build_faults().
bool tcc_recoverable_fault_config::keep |
Set to true
to enable keep action (keep until end of TCC cycle)
Referenced by _tcc_build_faults().
bool tcc_recoverable_fault_config::qualification |
Set to true
to enable input qualification (disable input when output is inactive)
Referenced by _tcc_build_faults().
bool tcc_recoverable_fault_config::restart |
Set to true
to enable restart action.
Referenced by _tcc_build_faults().
enum tcc_fault_source tcc_recoverable_fault_config::source |
Specifies if the event input generates recoverable Fault.
The event system channel connected to MCEx event input must be configured as asynchronous.
Referenced by _tcc_build_faults().