TC event enable/disable structure.
Event flags for the tc_enable_events() and tc_disable_events().
#include <tc.h>
Data Fields | |
enum tc_event_action | event_action |
Specifies which event to trigger if an event is triggered. More... | |
bool | generate_event_on_compare_channel [NUMBER_OF_COMPARE_CAPTURE_CHANNELS] |
Generate an output event on a compare channel match. More... | |
bool | generate_event_on_overflow |
Generate an output event on counter overflow. More... | |
bool | invert_event_input |
Specifies if the input event source is inverted, when used in PWP or PPW event action modes. More... | |
bool | on_event_perform_action |
Perform the configured event action when an incoming event is signalled. More... | |
enum tc_event_action tc_events::event_action |
Specifies which event to trigger if an event is triggered.
Referenced by tc_enable_events().
bool tc_events::generate_event_on_compare_channel[NUMBER_OF_COMPARE_CAPTURE_CHANNELS] |
Generate an output event on a compare channel match.
Referenced by tc_disable_events(), and tc_enable_events().
bool tc_events::generate_event_on_overflow |
Generate an output event on counter overflow.
Referenced by tc_disable_events(), and tc_enable_events().
bool tc_events::invert_event_input |
Specifies if the input event source is inverted, when used in PWP or PPW event action modes.
Referenced by tc_disable_events(), and tc_enable_events().
bool tc_events::on_event_perform_action |
Perform the configured event action when an incoming event is signalled.
Referenced by tc_disable_events(), and tc_enable_events().