Microchip® Advanced Software Framework

rtc_count_config Struct Reference

RTC Count configuration structure.

Configuration structure for the RTC instance. This structure should be initialized using the rtc_count_get_config_defaults() before any user configurations are set.

#include <rtc_count.h>

Data Fields

bool clear_on_match
 If true, clears the counter value on compare match. More...
 
uint32_t compare_values [RTC_NUM_OF_COMP16]
 Array of Compare values. More...
 
bool continuously_update
 Continuously update the counter value so no synchronization is needed for reading. More...
 
bool enable_read_sync
 Enable count read synchronization. More...
 
enum rtc_count_mode mode
 Select the operation mode of the RTC. More...
 
enum rtc_count_prescaler prescaler
 Input clock prescaler for the RTC module. More...
 

bool rtc_count_config::clear_on_match

If true, clears the counter value on compare match.

Only available whilst running in 32-bit mode

Referenced by _rtc_count_set_config(), configure_rtc(), and rtc_count_get_config_defaults().

uint32_t rtc_count_config::compare_values[RTC_NUM_OF_COMP16]

Array of Compare values.

Not all Compare values are available in 32-bit mode

Referenced by _rtc_count_set_config(), configure_rtc(), and rtc_count_get_config_defaults().

bool rtc_count_config::continuously_update

Continuously update the counter value so no synchronization is needed for reading.

Referenced by rtc_count_get_config_defaults().

bool rtc_count_config::enable_read_sync

Enable count read synchronization.

The COUNT value requires synchronization when reading. Disabling the synchronization will prevent the COUNT value from displaying the current value.

Referenced by _rtc_count_set_config(), and rtc_count_get_config_defaults().

enum rtc_count_mode rtc_count_config::mode

Select the operation mode of the RTC.

Referenced by _rtc_count_set_config(), configure_rtc(), rtc_count_get_config_defaults(), and rtc_count_init().

enum rtc_count_prescaler rtc_count_config::prescaler

Input clock prescaler for the RTC module.

Referenced by _rtc_count_set_config(), configure_rtc(), and rtc_count_get_config_defaults().