Microchip® Advanced Software Framework

Extra Information for ADC Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
ADC Analog-to-Digital Converter
DAC Digital-to-Analog Converter
LSB Least Significant Bit
MSB Most Significant Bit
DMA Direct Memory Access

Dependencies

This driver has the following dependencies:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Added support for SAM R21
Added support for SAM D21 and new DMA quick start guide
Added ADC calibration constant loading from the device signature row when the module is initialized
Initial Release