Microchip® Advanced Software Framework

Extra Information for PORT Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
GPIO General Purpose Input/Output
MUX Multiplexer

Dependencies

This driver has the following dependencies:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Added input event feature
Initial release