Overview:
Introduction
This unit test carries out tests for the TRNG driver.
It consists of test cases for the following functionalities:
- Test for TRNG polling mode read.
- Test for TRNG callback mode read.
The following kit is required for carrying out the test:
- SAM L21 Xplained Pro board
- SAM L22 Xplained Pro board
Setup
There is no special requirement.
To run the test:
- Connect the SAM Xplained Pro board to the computer using a micro USB cable.
- Open the virtual COM port in a terminal application.
- Note
- The USB composite firmware running on the Embedded Debugger (EDBG) will enumerate as debugger, virtual COM port, and EDBG data gateway.
- Build the project, program the target and run the application. The terminal shows the results of the unit test.
Usage
- Polling mode read is tested.
- Callback mode read is tested.
Compilation Info
This software was written for the GNU GCC and IAR for ARM. Other compilers may or may not work.
Contact Information
For further information, visit http://www.microchip.com.