NVM controller configuration structure.
Configuration structure for the NVM controller within the device.
#include <nvm.h>
Data Fields | |
enum nvm_cache_readmode | cache_readmode |
Select the mode for how the cache will pre-fetch data from the flash. More... | |
bool | disable_cache |
Setting this to true will disable the pre-fetch cache in front of the NVM controller. More... | |
bool | manual_page_write |
Manual write mode; if enabled, pages loaded into the NVM buffer will not be written until a separate write command is issued. More... | |
enum nvm_sleep_power_mode | sleep_power_mode |
Power reduction mode during device sleep. More... | |
uint8_t | wait_states |
Number of wait states to insert when reading from flash, to prevent invalid data from being read at high clock frequencies. More... | |
enum nvm_cache_readmode nvm_config::cache_readmode |
Select the mode for how the cache will pre-fetch data from the flash.
Referenced by nvm_get_config_defaults(), and nvm_set_config().
bool nvm_config::disable_cache |
Setting this to true will disable the pre-fetch cache in front of the NVM controller.
Referenced by nvm_get_config_defaults(), and nvm_set_config().
bool nvm_config::manual_page_write |
Manual write mode; if enabled, pages loaded into the NVM buffer will not be written until a separate write command is issued.
If disabled, writing to the last byte in the NVM page buffer will trigger an automatic write.
Referenced by eeprom_emulator_init(), nvm_get_config_defaults(), and nvm_set_config().
enum nvm_sleep_power_mode nvm_config::sleep_power_mode |
Power reduction mode during device sleep.
Referenced by nvm_get_config_defaults(), and nvm_set_config().
uint8_t nvm_config::wait_states |
Number of wait states to insert when reading from flash, to prevent invalid data from being read at high clock frequencies.
Referenced by nvm_get_config_defaults(), and nvm_set_config().