This simple example shows how to set up communication of the target MCU and Data Visualizer on PC.
All SAM devices can be used. This example has been tested with the following setup:
To run the test:
This example application will initiate communication with the Data Visualizer on the computer. Set up some elements on the dashboards, and some data stream between the target mcu and the computer.
This software was written for the GNU GCC and AtmelStudio. Other compilers may or may not work.
For further information, visit Microchip.