asynchronous mode
This example demonstrates using the FreeRTOS SPI driver to receive data using the fully asynchronous operation mode. See Initializing the FreeRTOS SPI driver
The example below implements a function that continuously processes previously received data while more data is being received.
This is a comprehensive quick start example and is intended for advanced users. It demonstrates the power and efficiency of the fully asynchronous API.
Refer to the FreeRTOS peripheral control projects in the Atmel ASF distribution for complete working examples, and the FreeRTOS web site for information on getting started with FreeRTOS.