standard mode
This example demonstrates using the FreeRTOS SPI driver to send data using the standard operation mode. See Initializing the FreeRTOS SPI driver
The example below implements a function that simply writes a block of data to an SPI port.
Refer to the FreeRTOS peripheral control projects in the Atmel ASF distribution for complete working examples, and the FreeRTOS web site for information on getting started with FreeRTOS.