fully asynchronous mode
This example demonstrates using the FreeRTOS TWI driver to send data using the fully asynchronous operation mode. See Initializing the FreeRTOS TWI driver
The example below implements a function that simply writes a block of data to a TWI port.
Refer to the FreeRTOS peripheral control projects in the Atmel ASF distribution for complete working examples, and the FreeRTOS web site for information on getting started with FreeRTOS.