fully asynchronous mode
This example demonstrates using the FreeRTOS USART API to send data using the fully asynchronous operation mode. See Initializing the FreeRTOS USART
The example below implements a function that transmits two strings, and then returns.
Refer to the FreeRTOS peripheral control projects in the Atmel ASF distribution for complete working examples, and the FreeRTOS web site for information on getting started with FreeRTOS.