BSD compatible socket interface between the host layer and the network protocol stacks in the firmware.
These functions are used by the host application to send or receive packets and to do other socket operations.
Modules | |
Defines | |
The following list of macros are used to define constants used throughout the socket layer, and SSL Socket options. | |
Byte Order | |
The following list of macros are used to convert between host representation and network byte order. | |
Error Codes | |
The following list of macros are used to define the possible error codes. | |
DataTypes | |
Specific Enumeration-typedefs used for socket operations. | |
Callbacks | |
Functions | |
The function performs the necessary initializations for the socket library through the following steps: | |