task.
h
void xTaskResumeFromISR( TaskHandle_t xTaskToResume );
INCLUDE_xTaskResumeFromISR must be defined as 1 for this function to be available. See the configuration section for more information.
An implementation of vTaskResume() that can be called from within an ISR.
A task that has been suspended by one or more calls to vTaskSuspend () will be made available for running again by a single call to xTaskResumeFromISR ().
xTaskResumeFromISR() should not be used to synchronise a task with an interrupt if there is a chance that the interrupt could arrive prior to the task being suspended - as this can lead to interrupts being missed. Use of a semaphore as a synchronisation mechanism would avoid this eventuality.
xTaskToResume | Handle to the task being readied. |
h
void xTaskResumeFromISR( xTaskHandle pxTaskToResume );
INCLUDE_xTaskResumeFromISR must be defined as 1 for this function to be available. See the configuration section for more information.
An implementation of vTaskResume() that can be called from within an ISR.
A task that has been suspended by one of more calls to vTaskSuspend () will be made available for running again by a single call to xTaskResumeFromISR ().
pxTaskToResume | Handle to the task being readied. |