Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
xTaskAbortDelay

task.

h

BaseType_t xTaskAbortDelay( TaskHandle_t xTask );

INCLUDE_xTaskAbortDelay must be defined as 1 in FreeRTOSConfig.h for this function to be available.

A task will enter the Blocked state when it is waiting for an event. The event it is waiting for can be a temporal event (waiting for a time), such as when vTaskDelay() is called, or an event on an object, such as when xQueueReceive() or ulTaskNotifyTake() is called. If the handle of a task that is in the Blocked state is used in a call to xTaskAbortDelay() then the task will leave the Blocked state, and return from whichever function call placed the task into the Blocked state.

Parameters
xTaskThe handle of the task to remove from the Blocked state.
Returns
If the task referenced by xTask was not in the Blocked state then pdFAIL is returned. Otherwise pdPASS is returned.