Resistive touch service settings for the ADS7843 controller.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "ads7843.h"
Macros | |
#define | rtouch_disable_interrupt() ads7843_disable_interrupt() |
ADS7843 touch driver specific function, see ads7843_disable_interrupt. More... | |
#define | rtouch_enable_interrupt() ads7843_enable_interrupt() |
ADS7843 touch driver specific function, see ads7843_enable_interrupt. More... | |
#define | rtouch_get_raw_point(p_x, p_y) ads7843_get_raw_point(p_x, p_y) |
ADS7843 touch driver specific function, see ads7843_get_raw_point. More... | |
#define | rtouch_init_device() ads7843_init() |
ADS7843 touch driver specific function, see ads7843_init. More... | |
#define | rtouch_is_pressed() ads7843_is_pressed() |
ADS7843 touch driver specific function, see ads7843_is_pressed. More... | |
#define | rtouch_set_handler(p_handler) ads7843_set_handler(p_handler) |
ADS7843 touch driver specific function, see ads7843_set_handler. More... | |