Microchip® Advanced Software Framework

mcps_data_conf_tag Struct Reference

This is the MCPS-DATA.confirm message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 < This identifies the message as MCPS_DATA_CONFIRM More...
 
uint8_t msduHandle
 The handle associated with the MSDU being confirmed. More...
 
uint8_t status
 The status of the last MSDU transmission. More...
 
uint32_t Timestamp
 Optional. More...