Microchip® Advanced Software Framework

mcps_purge_conf_tag Struct Reference

This is the MCPS-PURGE.confirm message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 < This identifies the message as MCPS_PURGE_CONFIRM More...
 
uint8_t msduHandle
 The handle of the MSDU requested to be purge from the transaction queue. More...
 
uint8_t status
 The status of the request to be purged an MSDU from the transaction queue. More...