Microchip® Advanced Software Framework

mlme_beacon_notify_ind_tag Struct Reference

This is the MLME-BEACON-NOTIFY.indication message structure.

#include <mac_msg_types.h>

Data Fields

uint8_t * AddrList
 The list of addresses of the devices for which the beacon source has data. More...
 
uint8_t BSN
 The beacon sequence number. More...
 
enum msg_code cmdcode
 This identifies the message as MLME_BEACON_NOTIFY_INDICATION. More...
 
wpan_pandescriptor_t PANDescriptor
 The PANDescriptor for the received beacon. More...
 
uint8_t PendAddrSpec
 The beacon pending address specification. More...
 
uint8_t * sdu
 The set of octets comprising the beacon payload to be transferred from the MAC sublayerentity to the next higher layer. More...
 
uint8_t sduLength
 The number of octets contained in the beacon payload of the beacon frame received by the MAC sublayer. More...