Microchip® Advanced Software Framework

mlme_comm_status_ind_tag Struct Reference

This is the MLME-COMM-STATUS.indication message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 This identifies the message as MLME_COMM_STATUS_INDICATION. More...
 
uint64_t DstAddr
 The individual device address of the device for which the frame was intended. More...
 
uint8_t DstAddrMode
 The destination addressing mode for this primitive. More...
 
uint16_t PANId
 The 16 bit PAN identifier of the device from which the frame was received or to which the frame was being sent. More...
 
uint64_t SrcAddr
 The source addressing mode for this primitive. More...
 
uint8_t SrcAddrMode
 The source addressing mode for this primitive. More...
 
uint8_t status
 The communications status. More...