Microchip® Advanced Software Framework

mlme_disassociate_conf_tag Struct Reference

This is the MLME-DISASSOCIATE.confirm message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 This identifies the message as MLME_DISASSOCIATE_CONFIRM. More...
 
uint64_t DeviceAddress
 The address of the device that has either requested disassociation or been instructed to disassociate by its coordinator. More...
 
uint8_t DeviceAddrMode
 The addressing mode of the device that has either requested disassociation or been instructed to disassociate by its coordinator. More...
 
uint16_t DevicePANId
 The PAN identifier of the device that has either requested disassociation or been instructed to disassociate by its coordinator. More...
 
uint8_t status
 The status of the disassociation attempt. More...