Microchip® Advanced Software Framework

mlme_disassociate_ind_tag Struct Reference

This is the MLME-DISASSOCIATE.indication message structure.

#include <mac_msg_types.h>

Data Fields

enum msg_code cmdcode
 This identifies the message as MLME_DISASSOCIATE_INDICATION. More...
 
uint64_t DeviceAddress
 The address of the device requesting disassociation. More...
 
uint8_t DisassociateReason
 The reason for the disassociation (see 7.3.1.3.2). More...